This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843AOP: How to arrange the order of output data through SPI?

Part Number: AWR1843AOP

Tool/software:

Hi,

I'm using SPI to transfer data.

Below, SPI setting

-------------------------------

Mode : SPI_MASTER

pinMode : SPI_PINMODE_4PIN_CS

dataSize : 16bit

frameFormat = SPI_POL0_PHA1

shiftFormat = SPI_MSB_FIRST

DMA : disable

csHold = 1

eccEnable = 1

transferMode = Blocking

 ------------------------------

When I send data and then receive it for verification, I observe that the data is swapped in 8-bit/8-bit units every 16 bits.

This issue does not occur when I set the data size to 8 bits and transmit the data.

I am curious if this data swapping is intentional and would like to know how to send the data without it being swapped.

Thanks.