Other Parts Discussed in Thread: AWR2944
Tool/software:
Hi,
I am setting up AWR2944EVM with DCA1000 capture card, in documents you're Setting up two different combinations of connection.
Setting - 1:
DCA - setting
1) FTDI and ethernet is connected to DCA1000.
2) SW3 is set to DC_JACK_5V_IN.
3) SW1 is set 12_bit_off, 14_bit_off and 16_bit_on.
4) SW2 is set LVDS_CAPT, DATA_MODE, SW_CONFIG, RAW_MODE.
5) 5V & 2.4amp supply is given.
AWR2944EVM
1) XDS110 is connected to AWR2944EVM.
2) S1 is set to XDS.
3) S2 is set PMIC
both is connected with 60pins samtec connector.
Setting - 2:
DCA - setting
1) Ethernet is connected to DCA1000.
2) SW3 is set to DC_JACK_5V_IN.
3) SW1 is set 12_bit_off, 14_bit_off and 16_bit_on.
4) SW2 is set LVDS_CAPT, DATA_MODE, SW_CONFIG, RAW_MODE.
5) 5V & 2.4amp supply is given.
AWR2944EVM
1) FTDI is connected to AWR2944EVM.
2) S1 is set to XDS.
3) S2 is set PMIC
both is connected with 60pins samtec connector.
I used setting - 1 and tried to connect to board by giving reset and RS232 connect but it failed not connecting with RS232, What should be used if I have to run and get data capture. lay your help on this.