This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: Re-flashing DCA1000EVM

Part Number: DCA1000EVM

Tool/software:

Dear TI experts,

I have several DCA1000EVM boards and am successfully using them with different TI radar.

However, one of the DCA1000EVM is not working with exact same setup which works with other DCA1000EVM boards.

All the drivers are installed, and DCA1000EVM has led light turned on at FPGA_DONE_LED and 5V_LED.

I tried to re-flash the not working DCA1000EVM with Lattice Diamond Programmer, but it gives an error. 

I followed same steps until 9.2.2 in DCA1000EVM Data Capture Card User's Guide (Rev. A).

2. The FPGA device (LFE5UM-85F) is detected in the programmer window, as shown in Figure 24.

Instead of LFE5UM-85F being detected, it is detected as Generic JTAG Device - JTAG-NOP.

Console output says like below 

Also, manually setting it to LFE5UM-85F fails later steps, saying Failed to verify the ID (Expected: 0x01113043 Read: 0xFFFFFFFF)

 

I have searched and read posts about same questions, but none of that worked for me.

Also link to https://processors.wiki.ti.com/images/3/3e/TMDXEVM3358-SK_FTDI_EEPROM_Programming_v1.1.pdf is not valid anymore showing Not-found error. 

How can I successfully re-flash the DCA1000EVM and use it again?

Best,