Tool/software:
Hello,
I'm using mmwave_diag SBL demo code from radar_box_1_10_00_13. I'm currently able to flash the application using SBL i have no issues doing it. However when i integrate I2C driver. i see RPRC failure when Image loader function is executed . Specifically here. However initiated I2C work fine. I'm able to read and write using the I2C. Can you please help me with the issue i'm facing. After I2C initialization i'm canceling and closing the i2c.
/* Load the input buffer to the RAM */
SBL_bufferMgmt((uint32_t*)gSblMCB.currBuff, SBL_PING_BUFFER_SIZE, 0);
Can you please let me know the allocated ROM memory size to flash SBL on AWR6843