This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMWCAS-RF-EVM: Telecommunications Standards

Part Number: MMWCAS-RF-EVM
Other Parts Discussed in Thread: AWR2243

Tool/software:

For the MMWCAS-RF-EVM that we purchased before, we are considering acquiring a special system to use it in experiments.
exp-sp.denpa.soumu.go.jp/.../

In order to receive the exception system, it is necessary to comply with one of the following standards set by the European Telecommunications Standards Organization.
Can you tell me if MMWCAS-RF-EVM (or AWR2243) is compliant with these standards?
ETSI EN 302 264
ETSI EN 303 360