Part Number: AWR2944EVM
Tool/software:
When I choose DDM in the Processing Chain, then the GUI prompts an error.
Can't DDM configure file be made in the DmmWave_Demo_Visualizer?
I want to make DDM configure file the DmmWave_Demo_Visualizer.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AWR2944EVM
Tool/software:
When I choose DDM in the Processing Chain, then the GUI prompts an error.
Can't DDM configure file be made in the DmmWave_Demo_Visualizer?
I want to make DDM configure file the DmmWave_Demo_Visualizer.
Hi Yuichi,
After setting the baudrate and connecting to the target, you can load one of the example configurations (.cfg) present in the mmwave_mcuplus_sdk_<ver>\ti\demo\<platform>\mmw\profiles folder and load it through the "LOAD CONFIG FROM PC AND SEND" button on the "Plots" tab.

Regards,
Samhitha
Hi,Samhitha
Thank you for reply.
Do you mean that DDM configure file can not be made in the mmWave_Demo_Visualizer?
I think TDM configure file can be madein in the mmWave_Demo_Visualize.
Regards,
Yuichi Morita
Hi Yuichi,
Do you mean that DDM configure file can not be made in the mmWave_Demo_Visualizer?
I didn't understand what you meant by making a config file in the demo visualizer. Do you mean sending the configuration to the device? If yes, then clicking "SEND CONFIG TO MMWAVE DEVICE" will send a default configuration i.e some TDM config. If you are running DDM demo and you want to configure the device, then you need to switch to "Plots" tab and click "LOAD CONFIG FROM PC AND SEND", choose the appropriate config file to send the configuration.

Regards,
Samhitha
Hi, Samhitha
Thank you for your understanding.
I think you can understand what I mean.
When I choose TDM in the Processing Chain,
I can set Scene Selection.

When I choose DDM in the Processing Chain,
I cannot set Scene Selection.

I want to know why I cannot set Scene Selection in DDM.
Regards,
Yuichi Morita
Hi Yuichi,
This feature is not supported for the DDM processing chain. You need to create your own configuration file.
Regards,
Samhitha