Tool/software:
When I am using the AWR2944EVM for the real time processing on the mmWave Demo Visualizer, then i am loading the Config file from the PC. In the config file, I have changed Tx = 1 , Rx = 1, that means I have made the transmitter and receiver equal to 1
But it is showing an Configuration error. Would you please tell me the reason for that?
Couldn't I set the number of Tx and Rx according to me. If it is so, then what are the possible combinations of the Tx and Rx channels for the demo visaulizer