Part Number: IWRL1432
Tool/software:
Dear experts, I encountered such a problem.
I got adc data ,like blow ( total 1024 points , I export adc data , and draw it)

then do fft with log use HWA ,get resluts below
There are alaways thress weird spikes. I am sure they are not real reflected signal.
(up curve is the result of doing it once. below curve is superimposed multiple times and some denoising and smoothing are done.)

This program is modified from the following program. use mmave sdk 05_03_00_02

The main parameters of chirp can be roughly expressed as follows using cli.
channelCfg 1 1 0
chirpComnCfg 8 5 0 1024 1 110 0
chirpTimingCfg 6 25 0 26.04 77.42
frameCfg 1 0 120 1 250 1
factoryCalibCfg 0 0 34 0 0x1ff000
What is the problem? Can you help me figure out how to solve it?
If you need any more information, feel free to ask me