Tool/software:
Hi Ti experts,
When I use your CPD demo GUI in radar tool box, I feel some confuse about the setting in vod_6843_aop_overhead_2row.
There are two profiledcfg command in this cfg, which are set for antenna 0 and antenna 1 and 2 respectively.
The different between them is the idle time, if I cancel the second profilecfg, the RF duty cycle increases to 230%.
In FCC, when the duty cycle is below 23%, we can use EIRP 14dBm rule.
So, can I cancel the first profieldcfg and setting the second profieldcfg to antenna 0 to get the low duty cycle?
What impact will this modification have on detection?
BR,
Vincent