Tool/software:
Hi,
In SDK 3.6, customer found below code at ti\drivers\gpio\include\reg_gio.h
/**
* @brief
* Only Ports A, B are capable of interrupts.
* This is a system limit on the GPIO IP Block
* for the devices supported so far.
*/
#define GPIO_MAX_INTERRUPT_PORT 2U
But in TRM, I only found there are 3 interrupts of GPIO. And there are 4 group of GPIO (A/B/C/D) which can enable for interrupts.
| VIM Interrupt Sources | Default VIM Interrupt Channel |
| MSS_GIO GPIO_0_host_interrupt | 18 |
| MSS_GIO GPIO_1_host_interrupt | 32 |
| MSS_GIO GPIO_2_host_interrupt | 48 |
The GPIO interrupt information are not matched. Would you pls help to check what I missed?
Thanks,
Chris