Other Parts Discussed in Thread: TCAN4550, AWRL1432, INA228
Tool/software:
Hi expert,
I enable CLI Bypass and configure parameter same with the profile_40m_40mpsec_boostevm_16tracks.cfg, meanwhile define TCAN4550(1) and use "CANFDLLD_MCANFrameType_CLASSIC" frametype.
When I debug the board (awrl1432_adas_bsd_demo_v2.2, MMWAVE_L_SDK_05_05_00_02), I find that the UART can output data normally, and the code can run into "TCAN4550_Transmit_Schedule" function, but I use Vector(set 500k baudrate) still can't get data from CAN, it made me confused, could you help me to confirm the problem?
BTW, I closed all INA228 relevant code, because if not, it will report error.

B.R.