Tool/software:
Hi,
DCA1000 receive data through LVDS, when would it start to stream data out through Ethernet? After one chirp received or one frame received?
Andy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi,
DCA1000 receive data through LVDS, when would it start to stream data out through Ethernet? After one chirp received or one frame received?
Andy
Hello,
The DCA1000 streams the data to the PC as it receives it with some small delay controlled by the user configurable packet delay. The packet delay will impact the overall throughput as described in the user guide.
There is also a 2GB DDR to temporarily store data in case the data input is faster than the Ethernet throughput. However, once this 2GB is full it will cause an error so you can only do short captures if the LVDS throughput is > the ethernet throughput to avoid overflowing the DDR memory.
Regards,
Adrian