Other Parts Discussed in Thread: IWR1443
Tool/software:
Drawings show IWRL1432 have two filters in each RX.
but in sdk can only set 1 HPF
/*!
* @brief Chirp Profile HPF corner frequency. This is a common HPF corner frequency value
* for all chirps in a frame. \n
* | Value | Definition |
* |---------|----------- |
* | 0 | 175kHz HPF corner frequency |
* | 1 | 350kHz HPF corner frequency |
* | 2 | 700kHz HPF corner frequency |
* | 3 | 1400kHz HPF corner frequency |
* Valid Range: 0 to 3
*/
UINT8 c_ChirpRxHpfSel;
Can I set up two?
————————
Compared with IWR1443, HPF1 and HPF2 can be set