Other Parts Discussed in Thread: INA226EVM, INA226
Tool/software:
Dear TI,
I found that one of TI-SCB (mark with D) very hot at the big IC when connecting to PC/USB hub.
Same setup, another TI-SCB (mark with B) do not feel the heat when connected to same PC/USB hub.
Beside, the Alert LED D2 INA226EVM (C) is also light up when connect to TI-SCB (D). Either of the INA226EVM connected to TI-SCB (D) also will trigger the Alert LED D2.
Serial communication to both TI-SCB currently is normal,
I believe it is not normal when the TI-SCB big IC at high temperature when connected to PC (even without connect to any EVM sensor board), kindly advise was the TI-SCB (D) is faulty or else how to debug so that the IC wont be at high temperature.