Tool/software:
Hello
I have a question about the AFE3010
My requirement is" GFI (Ground Fault Interruption) is performed by sensing the current flowing through both the live/hot and neutral lines. The current going out on the line must be equal to the returning current. If there is a difference, greater than 10mA, a fault is triggered and in less than 30mS the outlet will trip, meaning an electromechanical relay is opened and power is no longer present at the contacts."
I am well aware that UL943 only requires < 1 second. UL943 is not my requirement. Is there anyway to "speed" up the trip time with this device?
Thank you in advance