Tool/software:
Hi,
My customer is using I2C with slave transmitter mode in their system and got below waveform.
As you can see, each time after 8bits data were transmitted from slave, SCL was kept LOW for a while just before ACK from the master device.
Q1) According to TRM section 25.3.3 Slave Transmitter Mode, the I2C module hold the SCL pin Low when /XSMT=0.
Is this the situation described in the TRM?
Q2) The customer wants to remove or minimize the SCL=Low period.
To do so, transmit data need to be loaded to ICDXR register as fast as possible, correct?
Thanks and regards,
Koichiro Tashiro