Tool/software:
Hello,
I have a question about range bias and Rx channel gain/phase measurement by using "measureRangeBiasAndRxChanPhase".
The document* says, "The stated configuration profile (.cfg) must be used otherwise the calibration may not work as expected (this profile ensures all transmit and receive antennas are engaged among other things needed for calibration)."
There are several differences between the configuration for measurement and the configuration I want to use in the market.
For example, range resolution of the profile (profile_calibration.cfg) is 0.044m, but range resolution I plan to use in the market is 0.40 meters.
Is it acceptable for the chirp used for measurement to differ from the chirp I want to use in the market?
* C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/demo/xwr68xx/mmw/docs/doxygen/html/index.html
Regards,
Kei