This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi,
We want to use TMP126 with another SPI IC using the same SPI of the microcontroller.
Right now we have the follow:
But i don`t sure that work for the 10kohm resistor. Can we use the same SPI? or should we use two different SPI?
Best regards
Your schematic should work as-is assuming the other device's SDO/MISO is in a Z state when it is not addressed by the CS pin.
You could eliminate the 10kohm resistor by using TMP127, which doesn't require a MOSI connection to retrieve temperature data. This wouldn't have any impact on the above concern, of course.
ren