Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWRL6432AOPEVM: Assistance Required with fecDevicePowerOn Command Issue

Part Number: IWRL6432AOPEVM

Tool/software:

Hi,

I'm encountering issues with the fecDevicePowerOn command.

I’m using MMWAVE_L_SDK_05_04_00_01 and mmWave Studio 4.1.0.6.

The device is connected directly to the DCA1000, with the connections as shown here on page 20, plus an additional FTDI connection to the DCA1000. When I try to run the common_device_setup_60G.lua script, I receive the error below.

Could you please assist with this?

Thanks!

[12:56:13] [DFP API]xw_status=mws.fecDevicePowerOn(0,{h_XtalClkFreq=10240,c_ClkSourceSel=10,c_PowerMode=0,c_ChirpTimerResol=0,c_FecBootCfg=0,h_Reserved2=0,w_Reserved3=0})
[12:56:13] --xw_status: -112 (RFS_BOOT_TIMEOUT)
[12:56:13]
[12:56:13]
[12:56:13] &&&&&&&&&&&&&&&&&&&&
[12:56:13] ***Script FAILED!***
[12:56:13] &&&&&&&&&&&&&&&&&&&&
[12:56:13] Exception message is:
[12:56:13] ...labExamples\LUA_examples\common_device_setup_60G.lua:66: ERROR: API failed