Other Parts Discussed in Thread: AWR2544
Tool/software:
I've successfully used + flashed the mmwave out of box demo given provided meta image files. These work and are compatible with the 2544 visualization and CLI API. This metaImage includes valid recent MSS and BSS firmware which are shown with the version CLI command.
Separately, I've also successfully connected the DCA1000 and controlled and received data using the FTDI SPI control using mmwaveStudio 3. In this use case it appears I am forced to download the MSS and BSS firmware files at startup. If I attempt to control the board (in QSPI boot mode with above valid MSS+BSS) without loading this firmware, I receive a timeout/failed message response in the first command sent.
My question is this: Can I use the FTDI based SPI communication with a metaImage loaded MSS + BSS firmware ? So far I have only been able to use them independently. The MSS + BSS are loaded in flash, but it appears that FTDI SPI control no longer is able to communicate.
For example, if I wanted to control the awr2544EVM using only FTDI control, what metaImage needs to be flashed to the board to support this permanently? MMwaveStudio downloads it at each startup.
Thank you,
-Ross B