Tool/software:
Hi Team,
I'm working on the True ground speed detection lab from Radar Toolbox.
I would like to increase the signal strength of the Main lobe at boresight (forming angle at 0 degree) and attenuate the sidelobes.
In radar configuration, 'txPhaseShifter' is set to '0' value.
Are there additional configuration parameters available for increasing the Main Lobe signal strength, apart from the txPhaseShifter parameter?
Thanks
Mohan