Tool/software:
Hi,
I am using IWR6843 radar module. I have connected multiple radars (6 radars) on CAN bus. All radars are sending packets at 200ms time interval. I have observed few things mentioned below,
1. When I power on all radars at a time then I am not able to receive data from all the radars. Out of 6 sometime only 4 will work or 2 or sometimes all radars will work properly.
2. If I power on radars one by one then I am able to receive the data from all radars properly.
3. If I power on all radars and if I observe that I am not able to get the data properly from all the radars then I press on board reset button simultaneously and then it started receiving data from all the radars.
So is there any CAN bus arbitration issue that is affecting here in this case? Is it okay if I keep different packet transmitting rate of each radar like 200ms, 201ms, 202ms and so on? Or is there any CAN settting that I have to set in radar firmware?
Thanks,
Manoj