This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: What's the min clock frequency for SPI?

Part Number: AWR2243

Tool/software:

Hi,

What's the min clock frequency for the SPI interface which is used to communication with host?

I only found the max info in datasheet.

Thanks,

Chris

  • Hello,

    The AWR2243 is the SPI slave so the rate is defined by the host. The clock is generated by the master. The max rate is 40MHz, there is no spec for minimum rate. It depends on the host. 

    Regards,

    Adrian