Part Number: AWR2544LOPEVM
Other Parts Discussed in Thread: AWR2243BOOST
Tool/software:
Hi,
since the last thread is already closed i opened this one. You said it is possible that the AWR2544LOPEVM can be used in secondary mode and use the SYNC_IN (C17) function. Can you tell me how? In MMWave studio i can choose the hardware trigger option but it doesn't work. So i looked it up in the source code of the mss and i saw that the trigger option is delivered to the BSS. So i guess the BSS (RadarSS) is not using this option.
So can i get access to the source code of BSS? Then i can change it accordingly. If you don't want to share the code, can you maybe add this functionality?
The other option that was metioned was the Satellite architecture with PTP. Can you tell me what the timing accuracy is? I would need ~ns accuracy to be able to use it for MIMO processing with diffferent boards.
Best regards,
Oliver