This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWRL6432BOOST: radar cube size from IWRL6432BOOST + DCA1000

Part Number: IWRL6432BOOST


Tool/software:

Dear colleagues,

I use IWRL6432BOOST + DCA1000 and transfer data by means of Ethernet using mmWave Studio 4.1.0.6.

I use mmWaveSensingEstimator for radar parameters selection.

I see that the maximum possible radar cube size is 3*64*2*256, i.e. 64 samples per chirp and 256 chirps in a frame separately for Tx1 and Tx2 while using TDM.


Are there any possibilities to get bigger radar cube? At least 3*128*2*256 ?


Best regards,

Grigor Mardiyan