Tool/software:
Hello, I'm trying to find the captured ECHO signal on my oscilloscope, but I can't seem to point out the ECHO in the signal. I know the transducer (I'm using it in monostatic configuration) is bursting, because I can see it on my oscilloscope, and is listing because I can see it from the status bits. I used the speed of sound calculation to pinpoint the time the ECHO needs to return for an object that is 1 meter away. Time = distance /speed = 1 / 340 = 2941 us, this time can be seen on figure 3. So, any advice on how I can see the returned ECHO?
And I also get a lot of noise on the transducer pin that I can't get rid of. Is there a way to reduce the noise?
I send 16 pulses with 40 kHz frequency to the BOOSTXL-TUSS4470 module (see figure 1) and it is in IO_MODE 1.
And these are the register values:
BPF_CONFIG_1=0x00
BPF_CONFIG_2=0x00
DEV_CTRL_1=0x00
DEV_CTRL_2=0x05
DEV_CTRL_3=0x01
VDRV_CTRL=0x00
ECHO_INT_CONFIG=0x00
ZC_CONFIG=0x00
BURST_PULSE=0x10
TOF_CONFIG=0x00
Here the 16 pulses are seen on the + terminal of the transducer.
Here the noise can be seen, on the + terminal of the transducer.
Around this time, the returned ECHO needs to be seen according to the calculation.
Best regards,
Jarmo