This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: DCA1000 issue

Part Number: DCA1000EVM
Other Parts Discussed in Thread: IWR6843ISK

Tool/software:

I am using a DCA1000 with a IWR6843ISK board.  I am running mmWave Studio.  I seem to have random ability for the ethernet connection from the DCA1000 to PC making a connection to get RECORD turned on.  It seems to be random.  Sometimes, just power cycling the board works.  When it doesn't work, it says the command to the DCA1000 for it to go into RECORD mode timed out.  This happens a lot, and is very annoying.  I have used several different Windows PCs, and this happens on all of them.  I do not have issues with the USB interfaces.  Everything seems to work fine, there.  Please help. 

Regards,

Larry