Tool/software:
Hello,
I was playing around with the industrial visualizer and stored the data in a `.bin` format. I noticed that the number of points dropped periodically, while the same movement was performed. I set the maximum number of points to 150, and while most frames have 150 points in the pointclouds (and also as 'numDetectedpoints' in the OutputDict), Every ~10 frames, I have a frame with less points. As said the movement was identical during the data capturing. It felt a bit too rhythmical to be a coincidence.
Is this anything you encountered before, or can you maybe help me with a solution?
Demo: `3D people tracking`
Configuration: `AOP_6m_default`