Other Parts Discussed in Thread: TMAG6180
Tool/software:
Customer was using TDK TAS2142 for the position sensor for motor drive. Could you please help share the advantages of using TMAG6180-Q1 to compete it?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Customer was using TDK TAS2142 for the position sensor for motor drive. Could you please help share the advantages of using TMAG6180-Q1 to compete it?
Hi Aki,
Thank you for posting to the Sensors forum!
Please refer to the following E2E thread below which is essentially the same question, except the thread asks about the TDK TAS2143 device.
TMAG6180-Q1: What's the difference between AMR and TMR
Both the TAS2142 and the TAS2143 seem to be very similar devices with the primary difference being that the TAS2142 has a few specs that are a bit better than the TAS2143, notably the spec on angle accuracy across temperature. Even with the TAS2142 having improved angle accuracy when compared to the TAS2143, it is still comparable to the TMAG6180.
Best,
~Alicia