Other Parts Discussed in Thread: DXP, TMP422
Tool/software:
Hi All,
I am using the TMP422AMDCNTEP part for my design. Please clarify the below queries,
1) I am trying to use local temperature measurement alone not for remote sensor (So no Transistors are connected in my current design), So all the DX1,DX2,DX3,DX4 pins connected to ground through 4.64K ohms resistor.
Question:
1) If i connect the DX1,2,3,4 through 4.64k to ground will have issue?
2) As per datasheet DX2 and DX4 is DXN for slave address 0x4C , And datasheet recommends to unconnected . But if i connect through 4.64k to GND will have issue?
3) By connecting 4.64k ohms to GND on DX1,2,3,4 pins shall i able to configure I2C address as 0x4C?
Regards,
ANBARASU S