This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOP: timeout issue when trying to connect to DCA1000 from PC via static IP address

Part Number: IWR6843AOP
Other Parts Discussed in Thread: MMWAVE-STUDIO,

Tool/software:

Hi all,

we have several PC's (WIN11 and WIN10) that somehow cannot connect to the static IP address of the DCA1000 (stacking IWR6843AOP), and therefore timeout when the MMWAVE-STUDIO (v2.1.1.0) tries to connect to the DCA1000 FPGA.

From a board level of DCA1000/IWR6843AOP, we have one PC that is successfully connecting to the board with successful network connection, therefore the boards and FPGA firmware revision are functional.

Therefore we believe there is some kind of an issue with the PC allowing the network connection to the static IP address and port number potentially. Can you let us know which port number is being used or any other specifics to look out for when checking the PC configuration?

We are trying to make sure the PC is not for some reason blocking this network traffic.

Any ideas are greatly appreciated.

Thanks!

--Gunter