Tool/software:
Hi,
My customer is complaining 2 major issues in their system on TMP1827 :
- Major visible difference in the temperature from the sensor and ambiance temperature.
- Some time we see -ve values or huge number in between.
1.Major visible difference in the temperature from the sensor and ambiance temperature.
We configured the device for 12 bit precision and getting around 6 Degree Celsius difference from the ambiance temperature.
We tried with 16 bit precision by configuring “Device configuration -1” register for 16 bit but still didn’t see much difference .Below is the screenshot for your reference which we configured.

2.Some time we see -ve values or huge number in between.
To check the validity of the values for the sensor we read the checksum and calculated back to verify. Checksum was good for this -ve and huge values too.
We used the below sequence from the spec for the validation

Thanks,
Christina