Tool/software:
Hello,
I am trying to change the start frequency of the radar sensor. The range is 76GHZ - 81 GHZ , and I change the start frequency in the profile configuration and I launch the data collection process through ROS, and it launches a visualizer (RVIZ) that displays all of the point clouds that the sensor is detecting. However, once I change the start frequency above 77GHz I get an error and I can't see the point clouds. Could someone help me in changing the start frequency above 77GHz please.