This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMWCAS-DSP-EVM: Add linux use case for radar signal processing in Vision SDK

Part Number: MMWCAS-DSP-EVM


Tool/software:

Hello, we are using the MMWCAS-DSP-EVM and Vision SDK for radar application development.

Currently our software is based on the example application "tda2xx_cascade_linux_radar", it includes the linux usecases for cascade radar data collection. We would like to add the radar signal processing function into the software, and would like to add or modify a linux case to include the FFT function using EVE. However, I noticed that in Vision SDK, all the use cases for radar signal processing are rtos use cases, there is no linux use case for radar data processing...:(

May I ask if there is any example, which provides a linux use case, which includes the radar signal processing in Vision SDK? thank you very much!