Part Number: TMP112
Tool/software:
Hi team,
When testing the function of this temperature sensor, I found that there was an error of about three degrees between the data read by the software and the actual viscometric temperature line.
TMP112 is a local sensor and can only accurately measure the temperature under the IC. However, the customer's temperature measurement line is stuck in the middle of the sensor top surface. We cannot measure the temperature line directly under the IC. Is there any fixture that can measure it? Or can the two temperatures be converted?
Additionally, what else needs to be checked to confirm where the error comes from?
Thanks
Lillian