Tool/software:
Hi,
We are working on the Vital Signs with People Tracking demo and want to add a fall detection function on top of it, but there are two problems with the tracking function: (for Wall-mounted radar single-target detection and tracking)
1. Target tracking will always cause the tracking box cube to fly away, resulting in the loss of the target;
2. The tracking result of the radar output target pitch angle and the actual pitch angle are just opposite, when the actual target is below the radar level, the tracking result pitch angle is positive, and the tracking box cube is in a position above the radar level, when the actual target is above the radar level, the pitch angle of the tracking result is negative, and the tracking box cube is in a position that is biased below the radar level.
The above problem caused the fall detection function to not be carried out.
During the experiment, we flashed the "..\mmwave_industrial_toolbox_4_11_0\labs\People_Counting\3D_People_Counting\prebuilt_binaries\3D_people_count_68xx_demo.bin"to test fall detection, the tracking effect of this firmware is relatively stable, may I ask where the tracking problem in vital signs with people tracking is?
My profile for using vital signs with people tracking is given below: