This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: showing LVDS Buffer Full when trigger frame, FPGA ERROR LED glowing RED

Part Number: DCA1000EVM
Other Parts Discussed in Thread: AWR1843AOPEVM

Tool/software:

Hi Team,
I am working on AWR1843AOPEVM + DCA1000EVM to capture the ADC raw data.
1. In MM Wave studio it is showing error as "LVDS buffer full" and while trigger frame, FPGA error LED is glowing RED.
Please guide me resolve the issue.
2. During test, I observed that DDR3 got heat up too high. I done cold test, thinking DDR3 issue is there. May be this error because of DDR3 is not working. So, looking to replace it, but this IC is obsolete.  Please suggest an alternative part number for MT41K1G8SN-125 IT:A (DDR3 SDRAM).
 
Waiting for your response.
  • Hello,

    What is the power supply you are using? Did this board ever work in the past?

    Can you also share the full studio log when you see the error?

    Regards,

    Adrian

  • Yes, I have used the board in past time. I am giving power supply of 5V and 1 Amp to the DCA1000EVM board. For AWR1843AOPEVM power supply is through Laptop.

    The setup image providing here, please take look.

    Here the studio log when its showing error.

    GM: Constructor
    GM: Tue Oct 22 12:24:18 2024
    RSTD.Transmit("/Settings")
    [12:24:18]  
    [12:24:18]  ### Running Startup script: "C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\Scripts\Startup.lua" ###
    [12:24:18]  RSTD.SetAndTransmit ("/Settings/Scripter/Display DateTime" , "1")
    [12:24:18]  RSTD.SetAndTransmit ("/Settings/Scripter/DateTime Format" , "HH:mm:ss")
    [12:24:18]  Scripter ignored: Attempt to UnBuild() again or before Build.
    [12:24:18]  RSTD.SetVar ("/Settings/Clients/Client 0/Dll" , "C:\\ti\\mmwave_studio_02_01_01_00\\mmWaveStudio\\Clients\\\\LabClient.dll")
    [12:24:18]  RSTD.SetVar ("/Settings/Clients/Client 0/Use" , "TRUE")
    [12:24:18]  RSTD.SetVar ("/Settings/Clients/Client 1/Use" , "FALSE")
    [12:24:18]  RSTD.SetVar ("/Settings/Clients/Client 2/Use" , "FALSE")
    [12:24:18]  RSTD.SetVar ("/Settings/Clients/Client 3/Use" , "FALSE")
    [12:24:18]  RSTD.SetVar ("/Settings/Clients/Client 4/Use" , "FALSE")
    [12:24:18]  RSTD.SetVar ("/Settings/AL Client/AL Dll" , "C:\\ti\\mmwave_studio_02_01_01_00\\mmWaveStudio\\RunTime\\SAL.dll")
    [12:24:18]  RSTD.SetVar ("/Settings/Clients/Client 0/GuiDll" , "")
    [12:24:18]  RSTD.SetVar ("/Settings/AutoUpdate/Enabled" , "TRUE")
    [12:24:18]  RSTD.SetVar ("/Settings/AutoUpdate/Interval" , "1")
    [12:24:18]  RSTD.SetVar ("/Settings/Monitors/UpdateDisplay" , "TRUE")
    [12:24:18]  RSTD.SetVar ("/Settings/Monitors/OneClickStart" , "TRUE")
    [12:24:18]  RSTD.SetVar ("/Settings/Automation/Automation Mode" , "false")
    [12:24:18]  RSTD.Transmit("/")
    [12:24:18]  RSTD.SaveSettings(): Settings saved to "C:\Users\sshirsat\AppData\Roaming\RSTD\config.xml"
    [12:24:18]  RSTD.Build()
    [12:24:18]  RSTD.SaveSettings(): Settings saved to "C:\Users\sshirsat\AppData\Roaming\RSTD\config.xml"
    [12:24:18]  RSTD.Transmit("/")
    [12:24:18]  RSTD.AL_Build()
    [12:24:18]  RSTD.AL_LoadXml()
    [12:24:18]  RSTD.Transmit("/")
    [12:24:18]  RSTD.AL_Init()
    [12:24:18]  RSTD.Clients_Build()
    [12:24:18]  GM: Init
    [12:24:18]  GM: Loaded 'C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\Clients\\LabClient.dll'
    [12:24:18]  GM: 1 Guest (s) init
    [12:24:18]  GM: 1 Module(s) init
    [12:24:18]  GM: 2 Tab   (s) init
    [12:24:18]  RSTD.Client_LoadXml()
    [12:24:18]  [RadarAPI]: ar1.selectRadarMode(0)
    [12:24:18]  [RadarAPI]: Status: Passed
    [12:24:18]  Matlab Runtime Engine is installed
    [12:24:18]  [RadarAPI]: Starting Matlab Engine..
    [12:24:21]  [RadarAPI]: Matlab Engine Started!
    [12:24:22]  [RadarAPI]: ar1.selectCascadeMode(0)
    [12:24:22]  [RadarAPI]: Status: Passed
    [12:24:22]  [RadarAPI]: ar1.LoadSettings('C:\Users\sshirsat\AppData\Roaming\RSTD\ar1gui.ini')
    [12:24:23]  TESTING = false
    [12:24:23]  RstdNet: Port 2777: Listening..
    [12:24:23]  
    [12:24:23]  ***Script completed successfully.***
    [12:24:29]  [RadarAPI]: Opening Gpio Control Port()
    [12:24:29]  [RadarAPI]: Status: Passed
    [12:24:30]  [RadarAPI]: Opening Board Control Port()
    [12:24:30]  [RadarAPI]: Status: Passed
    [12:24:31]  [RadarAPI]: ar1.FullReset()
    [12:24:31]  [RadarAPI]: Status: Passed
    [12:24:32]  [RadarAPI]: Closing Board Control Port()
    [12:24:32]  [RadarAPI]: Status: Passed
    [12:24:32]  [RadarAPI]: Closing Gpio Control Port()
    [12:24:32]  [RadarAPI]: Status: Passed
    [12:24:32]  [RadarAPI]: ar1.SOPControl(2)
    [12:24:32]  [RadarAPI]: Status: Passed
    [12:24:40]  [RadarAPI]: ar1.Connect(15,921600,1000)
    [12:24:43]  [RadarAPI]: Warning: Connected with baudrate 115200
    [12:24:44]  [RadarAPI]: Warning: Disconnected existing BaudRate
    [12:24:44]  [RadarAPI]: Warning: Trying to connect with baudrate 921600
    [12:24:45]  [RadarAPI]: ar1.Calling_IsConnected()
    [12:24:47]  Device Status : UnDetDe/ASIL-B/SOP:2/ES:2
    [12:24:47]  [RadarAPI]: ar1.SaveSettings('C:\Users\sshirsat\AppData\Roaming\RSTD\ar1gui.ini')
    [12:24:50]  [RadarAPI]: ar1.frequencyBandSelection("77G")
    [12:24:54]  [RadarAPI]: ar1.SelectChipVersion("AR1642")
    [12:24:54]  [RadarAPI]: Status: Passed
    [12:24:54]  [RadarAPI]: ar1.deviceVariantSelection("XWR1843")
    [12:24:54]  [RadarAPI]: Status: Passed
    [12:24:57]  [RadarAPI]: ar1.DownloadBSSFw("C:\\ti\\mmwave_studio_02_01_01_00\\rf_eval_firmware\\radarss\\xwr18xx_radarss.bin")
    [12:24:57]  [RadarAPI]: Downloading BSS Patch RPRC Binary..
    [12:24:59]  [RadarAPI]: ar1.GetBSSFwVersion()
    [12:24:59]  [RadarAPI]: BSSFwVersion:(02.00.00.01 (05/10/17))
    [12:25:00]  [RadarAPI]: ar1.GetBSSPatchFwVersion()
    [12:25:00]  [RadarAPI]: BSSPatchFwVersion:(01.02.05.02 (30/04/19))
    [12:25:00]  [RadarAPI]: ar1.DownloadMSSFw("C:\\ti\\mmwave_studio_02_01_01_00\\rf_eval_firmware\\masterss\\xwr18xx_masterss.bin")
    [12:25:01]  [RadarAPI]: Downloading MSS RPRC Binary..
    [12:25:03]  [RadarAPI]: ar1.GetMSSFwVersion()
    [12:25:03]  [RadarAPI]: MSSFwVersion:(01.02.05.02 (16/07/19))
    [12:25:10]  [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0)
    [12:25:10]  [RadarAPI]: Status: Passed
    [12:25:10]  MSS power up done async event received!
    [12:25:18]  Device Status : UnDetDe/ASIL-B/SOP:2/ES:2
    [12:25:18]  [RadarAPI]: ar1.RfEnable()
    [12:25:18]  [RadarAPI]: Status: Passed
    [12:25:18]  BSS power up done async event received!
    [12:25:19]  [RadarAPI]: ar1.GetMSSFwVersion()
    [12:25:19]  [RadarAPI]: MSSFwVersion:(01.02.05.02 (16/07/19))
    [12:25:19]  [RadarAPI]: ar1.GetBSSFwVersion()
    [12:25:19]  [RadarAPI]: BSSFwVersion:(02.00.00.01 (05/10/17))
    [12:25:20]  [RadarAPI]: ar1.GetBSSPatchFwVersion()
    [12:25:20]  [RadarAPI]: BSSPatchFwVersion:(01.02.05.02 (30/04/19))
    [12:25:40]  [RadarAPI]: ar1.ChanNAdcConfig(1, 1, 0, 1, 1, 1, 1, 2, 1, 0)
    [12:25:40]  [RadarAPI]: Status: Passed
    [12:25:44]  [RadarAPI]: ar1.RfLdoBypassConfig(0x0)
    [12:25:44]  [RadarAPI]: Status: Passed
    [12:25:45]  [RadarAPI]: ar1.LPModConfig(0, 0)
    [12:25:45]  [RadarAPI]: Status: Passed
    [12:25:46]  [RadarAPI]: ar1.RfInit()
    [12:25:47]  RF Init async event received!
    [12:25:47]  [RadarAPI]: Status: Passed
    [12:25:47]  [RadarAPI]: Time stamp, Temperture: 28108,35; APLL Status, Update: 1, 0; SynthVCO1 Status, Update: 1, 1; SynthVCO2 Status, Update: 1, 1; LODist Status, Update: 1, 1; RxADCDC Status, Update: 1, 1; HPFcutoff Status, Update: 1, 1; LPFcutoff Status, Update: 1, 1; PeakDetector Status, Update: 1, 1; TxPower Status, Update: 1, 1; RxGain Status, Update: 1, 1; TxPhase Status, Update: 1, 1; RxIQMM Status, Update: 1, 1; 
    [12:25:51]  [RadarAPI]: ar1.SetMiscConfig(1)
    [12:25:51]  [RadarAPI]: Status: Passed
    [12:25:56]  [RadarAPI]: ar1.DataPathConfig(513, 1216644097, 0)
    [12:25:56]  [RadarAPI]: Status: Passed
    [12:25:58]  [RadarAPI]: ar1.LvdsClkConfig(1, 1)
    [12:25:58]  [RadarAPI]: Status: Passed
    [12:26:03]  [RadarAPI]: ar1.LVDSLaneConfig(0, 1, 1, 0, 0, 1, 0, 0)
    [12:26:03]  [RadarAPI]: Status: Passed
    [12:26:12]  [RadarAPI]: ar1.SetTestSource(4, 3, 0, 0, 0, 0, -327, 0, -327, 327, 327, 327, -2.5, 327, 327, 0, 0, 0, 0, -327, 0, -327, 327, 327, 327, -95, 0, 0, 0.5, 0, 1, 0, 1.5, 0, 0, 0, 0, 0, 0, 0)
    [12:26:12]  [RadarAPI]: Status: Passed
    [12:26:39]  [RadarAPI]: ar1.ProfileConfig(0, 77, 100, 6, 60, 0, 0, 0, 0, 0, 0, 29.982, 0, 256, 10000, 0, 0, 30)
    [12:26:39]  [RadarAPI]: Status: Passed
    [12:26:51]  [RadarAPI]: ar1.ChirpConfig(0, 0, 0, 0, 0, 0, 0, 1, 0, 0)
    [12:26:51]  [RadarAPI]: Status: Passed
    [12:26:55]  Test Source Already Disabled...!!!
    [12:26:55]  [RadarAPI]: ar1.DisableTestSource(0)
    [12:26:55]  [RadarAPI]: Status: Passed
    [12:26:55]  [RadarAPI]: ar1.FrameConfig(0, 0, 8, 128, 40, 0, 0, 1)
    [12:26:55]  [RadarAPI]: Status: Passed
    [12:27:00]  [RadarAPI]: ar1.GetCaptureCardDllVersion()
    [12:27:00]  [RadarAPI]: Sending dll_version command to DCA1000
    [12:27:00]  [RadarAPI]: 
    [12:27:00]  DLL Version : 1.0
    [12:27:00]  [RadarAPI]: ar1.SelectCaptureDevice("DCA1000")
    [12:27:00]  [RadarAPI]: Status: Passed
    [12:27:07]  [RadarAPI]: ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "12:34:56:78:90:12", 4096, 4098)
    [12:27:07]  [RadarAPI]: ar1.CaptureCardConfig_Mode(1, 2, 1, 2, 3, 30)
    [12:27:07]  [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25)
    [12:27:07]  [RadarAPI]: Sending fpga command to DCA1000
    [12:27:07]  [RadarAPI]: 
    [12:27:07]  FPGA Configuration command : Success
    [12:27:07]  [RadarAPI]: Sending record command to DCA1000
    [12:27:08]  [RadarAPI]: 
    [12:27:08]  Configure Record command : Success
    [12:27:08]  [RadarAPI]: ar1.GetCaptureCardFPGAVersion()
    [12:27:08]  [RadarAPI]: Sending fpga_version command to DCA1000
    [12:27:08]  [RadarAPI]: 
    [12:27:08]  
    [12:27:08]  FPGA Version : 2.8 [Record]
    [12:27:08]  
    [12:27:58]  [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_02_01_01_00\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
    [12:27:58]  [RadarAPI]: Sending start_record command to DCA1000
    [12:28:01]  [RadarAPI]: ar1.StartFrame()
    [12:28:01]  [RadarAPI]: Status: Passed
    [12:28:01]  Frame start async event received!
    [12:28:01]  Frame End async event received!
    [12:28:01]  [RadarAPI]: Frame Ended
    [12:29:20]  [RadarAPI]: 
    [12:29:20]  [RadarAPI]: 
    [12:29:20]  Start Record command : Success
    [12:29:20]  
    [12:29:20]  LVDS buffer full
    [12:29:20]  
    [12:29:20]  Record Process : 
    [12:29:20]  Timeout Error! System disconnected
    [12:29:20]  
    [12:29:20]  Record stop is done successfully
    

    Meanwhile if you could suggest the alternative for DDR3 it will be helpful?

  • Hello,

    Based on your log it looks like there is something wrong with your DCA1000. You are getting overflow message which means the data is not being sent out over Ethernet fast enough, but your configuration should not cause this issue. So, it seems like there is some issue with the DCA1000 failing to send data over Ethernet. 

    I would recommend following the customer return process below based on where you purchased the board. Then, you can provide them a link to this thread as evidence. They should provide you with a replacement for free.

    Customer returns | Additional information | TI.com

    Regards,

    Adrian