Tool/software:
Most ASICs designed for metal target inductive sensors allow for connecting two chips to the same excitation coil. Each sensor can measure its own set of receive coils. For instance, one set can be configured for a fine scale and another for a coarse scale. Can two LDC5071 parts be connected to the same pair of capacitors and the same single excitation coil? Additionally, do we need to use four resistors, approximately 10 Ohms each, on the LCin and LCout pins of each LDC5071 to isolate them? Thank you! Any feedback would be greatly appreciated.