Tool/software:
Hi,
I have a space-constrained application where the coil assembly must fit within a 6 mm diameter cylindrical hole. If I use a 4-layer PCB coil, there isn't room for the tank capacitor in-plane. Is it acceptable to mount the capacitor slightly away from the coil, in say a perpendicular orientation? I assume that it isn't a good idea to place the capacitor in the center of the coil?
Are there any recommended wire-wound inductors that meet the crisscrossed winding requirement? I have flexibility in the air gap dimension. Can I house the sensor assembly in a metal tube without degrading the performance of the system?
Thanks!