This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944: detection of UAV

Part Number: AWR2944
Other Parts Discussed in Thread: AWR1843

Tool/software:

Hi, experts 

I want to use AWR2944 or any radar chips suggested by TI to do the UAV detection. The equipment is located on the ground.

I know AWR2944 is prefered for vehicle products. Not sure it is usable for UAV detection or any solution from TI for UAV detection is available? 

Can TI give a solution to satisfy the requirements below ?

My requirements are listed here:

1. rang of height of UAV that will be detected :  <=120m

2. RCS ~0.04m2 (unit : square meter)

3. range of speed of UAV that will be detected: from 1-2m/s to 20~30m/s 

thanks , any feedback to chenhao48@asiainfo.com is appreciated!