This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK: Measuring Higher doppler values

Part Number: IWR6843ISK
Other Parts Discussed in Thread: IWR6843

Tool/software:

Hi, We are using the IWR6843 chip to measure air velocity, where the actual air velocity is approximately 344 m/s. However, with our current configuration, the Nyquist velocity limit is set to 30 m/s. How can we accurately interpret such high velocities from our recorded data? If velocity folding (or aliasing) occurs across Doppler bins due to this limitation, will there be any bin error introduced with each fold?