This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944EVM: The adopted waveform parameters result in the phenomenon of chirp data loss in AD sampling when debug in mmWaveStudio

Part Number: AWR2944EVM
Other Parts Discussed in Thread: AWR2944

Tool/software:

Hi,

When debugging with the AWR2944, sampling works normally with the official default parameters.

However, when using custom-configured waveform parameters, it was observed through the mmWaveStudio host operation that the acquired AD data exhibits chirp data loss.

This is characterized by consecutive missing chirps across all four receiving channels corresponding to each frame of data.

The configuration of the waveform parameters is as follows:

A single waveform has been configured, enabling the channel tx1. Each frame consists of 128 chirps, with a frame period of 40 ms, and a total of 20 frames are transmitted. The four receiving channels rx1-4 simultaneously acquire AD data. Post-processing results show that the signals for the 8th to 13th chirps on rx1 are missing or completely lost.

The following figure presents the sampling results for the 8th chirp on rx1, revealing that some sampling data is missing.

The following figure presents the sampling results for the 9th chirp on rx1, revealing that all sampling data is missing.

Except for the 9th chirp, the data for the 10th, 11th, and 12th chirps is also missing.

The following figure presents the sampling results for the 13th chirp on rx1, revealing that part of sampling data is missing.

We attempted to change the idletime to 60μs, which resolved the issue, but we are still unclear about the underlying cause. Additionally, we do not wish to change this parameter. How should we analyze this problem? Thank you very much for your response.

Regards,

Liliang

  • Hello,

    I don't see anything wrong with your configuration that should cause this issue. 

    Can you compare the file size of the working case (60 us idle) to the failing case? If they are both the same size then most likely it is some kind of bug in the post processing tool and not an actual capture issue. 

    Can you also please share the full mmwave studio output log from start to end so I can replicate the exact same thing on my end?

    Regards,

    Adrian

  • Hello, thank you for your response.

    Based on the configured waveform, we verified that the data size is correct. To determine if there was an error in post-processing, we wrote a MATLAB script to read the data ourselves and found that it was consistent with the issue we reported earlier: the data values in the missing chirp sections were all zero. Additionally, to further investigate, we conducted the same test using another board and observed the same phenomenon. I have also attached the log file.

    GM: Constructor
    GM: Fri Nov 01 13:22:51 2024
    RSTD.Transmit("/Settings")
    [13:22:53]  
    [13:22:53]  ### Running Startup script: "C:\ti\mmwave_studio_03_01_03_01\mmWaveStudio\Scripts\Startup.lua" ###
    [13:22:53]  RSTD.SetAndTransmit ("/Settings/Scripter/Display DateTime" , "1")
    [13:22:53]  RSTD.SetAndTransmit ("/Settings/Scripter/DateTime Format" , "HH:mm:ss")
    [13:22:53]  Scripter ignored: Attempt to UnBuild() again or before Build.
    [13:22:53]  RSTD.SetVar ("/Settings/Clients/Client 0/Dll" , "C:\\ti\\mmwave_studio_03_01_03_01\\mmWaveStudio\\Clients\\\\LabClient.dll")
    [13:22:53]  RSTD.SetVar ("/Settings/Clients/Client 0/Use" , "TRUE")
    [13:22:53]  RSTD.SetVar ("/Settings/Clients/Client 1/Use" , "FALSE")
    [13:22:53]  RSTD.SetVar ("/Settings/Clients/Client 2/Use" , "FALSE")
    [13:22:53]  RSTD.SetVar ("/Settings/Clients/Client 3/Use" , "FALSE")
    [13:22:53]  RSTD.SetVar ("/Settings/Clients/Client 4/Use" , "FALSE")
    [13:22:53]  RSTD.SetVar ("/Settings/AL Client/AL Dll" , "C:\\ti\\mmwave_studio_03_01_03_01\\mmWaveStudio\\RunTime\\SAL.dll")
    [13:22:53]  RSTD.SetVar ("/Settings/Clients/Client 0/GuiDll" , "")
    [13:22:53]  RSTD.SetVar ("/Settings/AutoUpdate/Enabled" , "TRUE")
    [13:22:53]  RSTD.SetVar ("/Settings/AutoUpdate/Interval" , "1")
    [13:22:53]  RSTD.SetVar ("/Settings/Monitors/UpdateDisplay" , "TRUE")
    [13:22:53]  RSTD.SetVar ("/Settings/Monitors/OneClickStart" , "TRUE")
    [13:22:53]  RSTD.SetVar ("/Settings/Automation/Automation Mode" , "false")
    [13:22:53]  RSTD.Transmit("/")
    [13:22:53]  RSTD.SaveSettings(): Settings saved to "C:\Users\Administrator\AppData\Roaming\RSTD\config.xml"
    [13:22:53]  RSTD.Build()
    [13:22:53]  RSTD.SaveSettings(): Settings saved to "C:\Users\Administrator\AppData\Roaming\RSTD\config.xml"
    [13:22:53]  RSTD.Transmit("/")
    [13:22:53]  RSTD.AL_Build()
    [13:22:53]  RSTD.AL_LoadXml()
    [13:22:53]  RSTD.Transmit("/")
    [13:22:53]  RSTD.AL_Init()
    [13:22:53]  RSTD.Clients_Build()
    [13:22:53]  GM: Init
    [13:22:53]  GM: Loaded 'C:\ti\mmwave_studio_03_01_03_01\mmWaveStudio\Clients\\LabClient.dll'
    [13:22:53]  GM: 1 Guest (s) init
    [13:22:53]  GM: 1 Module(s) init
    [13:22:53]  GM: 2 Tab   (s) init
    [13:22:53]  RSTD.Client_LoadXml()
    [13:22:53]  [RadarAPI]: ar1.GuiVersion()
    [13:22:53]  [RadarAPI]: ar1.selectRadarMode(0)
    [13:22:53]  [RadarAPI]: Status: Passed
    [13:22:53]  Matlab Runtime Engine is installed
    [13:22:53]  [RadarAPI]: Starting Matlab Engine..
    [13:22:55]  [RadarAPI]: Matlab Engine Started!
    [13:22:57]  [RadarAPI]: ar1.selectCascadeMode(0)
    [13:22:57]  [RadarAPI]: Status: Passed
    [13:22:57]  [RadarAPI]: ar1.LoadSettings('C:\Users\Administrator\AppData\Roaming\RSTD\ar1gui.ini')
    [13:22:57]  TESTING = false
    [13:22:57]  RstdNet: Port 2777: Listening..
    [13:22:57]  
    [13:22:57]  ***Script completed successfully.***
    [13:23:03]  LuaLoad("F:/dns_liliang/LUAScript/new_DataCapture_2944_test.lua")
    [13:23:04]  [RadarAPI]: Opening Board Control Port()
    [13:23:04]  [RadarAPI]: Status: Passed
    [13:23:05]  [RadarAPI]: ar1.FullReset()
    [13:23:05]  [RadarAPI]: Status: Failed To give full reset, Error Value: -7
    [13:23:05]  [RadarAPI]: Closing Board Control Port()
    [13:23:05]  [RadarAPI]: Status: Passed
    [13:23:05]  [RadarAPI]: Opening Gpio Control Port()
    [13:23:05]  [RadarAPI]: Status: Passed
    [13:23:06]  [RadarAPI]: Opening Board Control Port()
    [13:23:06]  [RadarAPI]: Status: Passed
    [13:23:07]  [RadarAPI]: ar1.FullReset()
    [13:23:07]  [RadarAPI]: Status: Passed
    [13:23:08]  [RadarAPI]: Closing Board Control Port()
    [13:23:08]  [RadarAPI]: Status: Passed
    [13:23:08]  [RadarAPI]: Closing Gpio Control Port()
    [13:23:08]  [RadarAPI]: Status: Passed
    [13:23:08]  [RadarAPI]: ar1.SOPControl(2)
    [13:23:08]  [RadarAPI]: Status: Passed
    [13:23:08]  [RadarAPI]: ar1.Connect(14,921600,1000)
    [13:23:10]  [RadarAPI]: Warning: Connected with baudrate 115200
    [13:23:12]  [RadarAPI]: Warning: Disconnected existing BaudRate
    [13:23:12]  [RadarAPI]: Warning: Trying to connect with baudrate 921600
    [13:23:13]  [RadarAPI]: ar1.Calling_IsConnected()
    [13:23:15]  [RadarAPI]: Part number of the device = 0x98
    [13:23:15]  [RadarAPI]: Device type = GP
    [13:23:15]  [RadarAPI]: ar1.SelectChipVersion("AR1642")
    [13:23:15]  [RadarAPI]: Status: Passed
    [13:23:15]  [RadarAPI]: ar1.deviceVariantSelection("XWR2944")
    [13:23:15]  [RadarAPI]: Status: Passed
    [13:23:15]  [RadarAPI]: ar1.frequencyBandSelection("77G")
    [13:23:15]  [RadarAPI]: ar1.SelectChipVersion("AWR2944")
    [13:23:15]  [RadarAPI]: Status: Passed
    [13:23:15]  Device Status : AWR2944/GP/ASIL-B/SOP:2/ES:2.0
    [13:23:15]  [RadarAPI]: ar1.Calling_IsConnected()
    [13:23:16]  [RadarAPI]: Part number of the device = 0x98
    [13:23:16]  [RadarAPI]: Device type = GP
    [13:23:16]  [RadarAPI]: ar1.SelectChipVersion("AWR2944")
    [13:23:16]  [RadarAPI]: Status: Passed
    [13:23:16]  Device Status : AWR2944/GP/ASIL-B/SOP:2/ES:2.0
    [13:23:16]  [RadarAPI]: ar1.SelectChipVersion("AR1642")
    [13:23:16]  [RadarAPI]: Status: Passed
    [13:23:16]  [RadarAPI]: ar1.frequencyBandSelection("77G")
    [13:23:16]  [RadarAPI]: ar1.SelectChipVersion("AR1642")
    [13:23:16]  [RadarAPI]: Status: Passed
    [13:23:16]  [RadarAPI]: ar1.DownloadBSSFw("F:\\ti\\mmwave_studio_03_01_03_01\\rf_eval_firmware\\radarss\\xwr29xx_radarss_rprc.bin")
    [13:23:20]  [RadarAPI]: ar1.GetBSSFwVersion()
    [13:23:20]  [RadarAPI]: BSSFwVersion:(02.04.05.03 (20/04/22))
    [13:23:21]  [RadarAPI]: ar1.GetBSSPatchFwVersion()
    [13:23:21]  [RadarAPI]: BSSPatchFwVersion:(02.04.09.05 (28/06/23))
    [13:23:22]  [RadarAPI]: ar1.DownloadMSSFw("F:\\ti\\mmwave_studio_03_01_03_01\\rf_eval_firmware\\masterss\\xwr2xxx_masterss.bin")
    [13:23:24]  [RadarAPI]: Downloading MSS RPRC Binary..
    [13:23:29]  [RadarAPI]: ar1.GetMSSFwVersion()
    [13:23:29]  [RadarAPI]: MSSFwVersion:(02.04.02.12 (05/01/24))
    [13:23:29]  [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0)
    [13:23:29]  [RadarAPI]: Status: Passed
    [13:23:29]  MSS power up done async event received!
    [13:23:29]  [RadarAPI]: ar1.RfEnable()
    [13:23:29]  BSS power up done async event received!
    [13:23:29]  [RadarAPI]: Status: Passed
    [13:23:30]  [RadarAPI]: ar1.GetMSSFwVersion()
    [13:23:30]  [RadarAPI]: MSSFwVersion:(02.04.02.12 (05/01/24))
    [13:23:30]  [RadarAPI]: ar1.GetBSSFwVersion()
    [13:23:30]  [RadarAPI]: BSSFwVersion:(02.04.05.03 (20/04/22))
    [13:23:31]  [RadarAPI]: ar1.GetBSSPatchFwVersion()
    [13:23:31]  [RadarAPI]: BSSPatchFwVersion:(02.04.09.05 (28/06/23))
    [13:23:32]  [RadarAPI]: ar1.ChanNAdcConfig(1, 1, 0, 0, 1, 1, 1, 1, 2, 0, 0)
    [13:23:32]  [RadarAPI]: Status: Passed
    [13:23:32]  [RadarAPI]: ar1.LPModConfig(0, 0)
    [13:23:32]  [RadarAPI]: Status: Passed
    [13:23:32]  [RadarAPI]: ar1.RfInit()
    [13:23:33]  RF Init async event received!
    [13:23:33]  [RadarAPI]: Time stamp, Temperture: 3015,36; SynthVCO3 Status, Update: 0, 0; APLL Status, Update: 1, 0; SynthVCO1 Status, Update: 1, 1; SynthVCO2 Status, Update: 1, 1; LODist Status, Update: 1, 1; RxADCDC Status, Update: 1, 1; HPFcutoff Status, Update: 1, 1; LPFcutoff Status, Update: 1, 1; PeakDetector Status, Update: 1, 1; TxPower Status, Update: 1, 1; RxGain Status, Update: 1, 1; TxPhase Status, Update: 1, 1; RxIQMM Status, Update: 0, 0; 
    [13:23:33]  [RadarAPI]: Status: Passed
    [13:23:33]  [RadarAPI]: ar1.DataPathConfig(513, 1216644097, 0)
    [13:23:33]  [RadarAPI]: Status: Passed
    [13:23:33]  [RadarAPI]: ar1.LVDSLaneConfig(0, 1, 1, 0, 0, 1, 0, 0)
    [13:23:33]  [RadarAPI]: Status: Passed
    [13:23:33]  [RadarAPI]: ar1.SetTestSource(4, 3, 0, 0, 0, 0, -327, 0, -327, 327, 327, 327, -2.5, 327, 327, 0, 0, 0, 0, -327, 0, -327, 327, 327, 327, -95, 0, 0, 0.5, 0, 1, 0, 1.5, 0, 0, 0, 0, 0, 0, 0, 0)
    [13:23:33]  [RadarAPI]: Status: Passed
    [13:23:33]  [RadarAPI]: ar1.ProfileConfig(0, 80.000000006, 6, 4, 20, 0, 0, 0, 0, 0, 0, 0, 0, 3.042, 0, 256, 17000, 2216755200, 0, 158, 0, 0, 0)
    [13:23:33]  [RadarAPI]: Status: Passed
    [13:23:33]  [RadarAPI]: ar1.ChirpConfig(0, 0, 0, 0, 0, 0, 0, 1, 0, 0, 0)
    [13:23:33]  [RadarAPI]: Status: Passed
    [13:23:33]  [RadarAPI]: ar1.EnableTestSource(1)
    [13:23:33]  [RadarAPI]: Status: Passed
    [13:23:33]  [RadarAPI]: ar1.DisableTestSource(0)
    [13:23:33]  [RadarAPI]: Status: Passed
    [13:23:33]  [RadarAPI]: ar1.AdvanceFrameConfig(4, 1536, 0, 0, 1, 255, 1600000, 0, 1, 3, 5000000, 0, 0, 1, 255, 1600000, 0,1, 3, 5000000, 0, 0, 1, 255, 1600000, 0, 1, 3, 5000000, 0, 0, 1, 255,1600000, 0, 1, 3, 5000000, 64, 1, 0, 4, 765, 256, 1, 765, 256, 1, 765,256, 1, 765, 256, 1)
    [13:23:33]  [RadarAPI]: Status: Passed
    [13:23:33]  [RadarAPI]: ar1.GetCaptureCardDllVersion()
    [13:23:33]  [RadarAPI]: Sending dll_version command to DCA1000
    [13:23:33]  [RadarAPI]: 
    [13:23:33]  DLL Version : 1.0
    [13:23:33]  [RadarAPI]: ar1.SelectCaptureDevice("DCA1000")
    [13:23:33]  [RadarAPI]: Status: Passed
    [13:23:33]  [RadarAPI]: ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "c:22:38:4e:5a:c", 4096, 4098)
    [13:23:33]  [RadarAPI]: Sending fpga command to DCA1000
    [13:23:34]  [RadarAPI]: 
    [13:23:34]  
    [13:23:34]  
    [13:23:34]  ConfigureRFDCCard_Mode(): UDP write failed : 10051
    [13:23:34]  FPGA Configuration : 
    [13:23:34]  Sending command failed - -3
    [13:23:34]  [RadarAPI]: Sending fpga_version command to DCA1000
    [13:23:34]  [RadarAPI]: 
    [13:23:34]  
    [13:23:34]  
    [13:23:34]  ReadRFDCCard_FpgaVersion(): UDP write failed : 10051
    [13:23:34]  
    [13:23:34]  [RadarAPI]: ar1.CaptureCardConfig_Mode(1, 2, 1, 2, 3, 0)
    [13:23:34]  [RadarAPI]: Sending fpga command to DCA1000
    [13:23:34]  [RadarAPI]: 
    [13:23:34]  
    [13:23:34]  
    [13:23:34]  ConfigureRFDCCard_Mode(): UDP write failed : 10051
    [13:23:34]  FPGA Configuration : 
    [13:23:34]  Sending command failed - -3
    [13:23:34]  [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25)
    [13:23:34]  [RadarAPI]: Sending fpga command to DCA1000
    [13:23:34]  [RadarAPI]: 
    [13:23:34]  
    [13:23:34]  
    [13:23:34]  ConfigureRFDCCard_Mode(): UDP write failed : 10051
    [13:23:34]  FPGA Configuration : 
    [13:23:34]  Sending command failed - -3
    [13:23:34]  [RadarAPI]: Sending record command to DCA1000
    [13:23:34]  [RadarAPI]: 
    [13:23:34]  
    [13:23:34]  
    [13:23:34]  ConfigureRFDCCard_Record(): UDP write failed : 10051
    [13:23:34]  Configure Record : 
    [13:23:34]  Sending command failed - -3
    [13:23:34]  [RadarAPI]: ar1.GetCaptureCardFPGAVersion()
    [13:23:34]  [RadarAPI]: Sending fpga_version command to DCA1000
    [13:24:04]  [RadarAPI]: 
    [13:24:04]  
    [13:24:04]  
    [13:24:04]  ReadRFDCCard_FpgaVersion(): UDP write failed : 10051
    [13:24:04]  
    [13:24:04]  [RadarAPI]: ar1.CaptureCardConfig_StartRecord("F:\\ti\\mmwave_studio_03_01_03_01\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
    [13:24:04]  [RadarAPI]: Sending start_record command to DCA1000
    [13:24:04]  [RadarAPI]: Status: Passed
    [13:24:04]  RSTD.ShowLogFile()
    [13:24:04]  
    [13:24:04]  ***Script completed successfully.***
    [13:24:59]  [RadarAPI]: ar1.CaptureCardConfig_StartRecord("F:\\ti\\mmwave_studio_03_01_03_01\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
    [13:24:59]  [RadarAPI]: Sending start_record command to DCA1000
    [13:25:00]  [RadarAPI]: 
    [13:25:00]  
    [13:25:00]  
    [13:25:00]  StartRecordData(): UDP write failed : 10051
    [13:25:00]  Start Record : 
    [13:25:00]  Sending command failed - -3
    [13:25:35]  [RadarAPI]: ar1.CaptureCardConfig_StartRecord("F:\\ti\\mmwave_studio_03_01_03_01\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
    [13:25:35]  [RadarAPI]: Sending start_record command to DCA1000
    [13:25:35]  [RadarAPI]: 
    [13:25:35]  
    [13:25:35]  
    [13:25:35]  StartRecordData(): UDP write failed : 10051
    [13:25:35]  Start Record : 
    [13:25:35]  Sending command failed - -3
    [13:26:54]  LuaLoad("F:/dns_liliang/LUAScript/new_DataCapture_2944_test.lua")
    [13:26:54]  [RadarAPI]: ar1.Disconnect()
    [13:26:54]  [RadarAPI]: ar1.Calling_ATE_DisconnectTarget()
    [13:26:54]  [RadarAPI]: ar1.Calling_IsConnected()
    [13:26:54]  [RadarAPI]: ar1.SaveSettings('C:\Users\Administrator\AppData\Roaming\RSTD\ar1gui.ini')
    [13:26:55]  [RadarAPI]: Opening Board Control Port()
    [13:26:55]  [RadarAPI]: Status: Passed
    [13:26:56]  [RadarAPI]: ar1.FullReset()
    [13:26:56]  [RadarAPI]: Status: Passed
    [13:26:56]  [RadarAPI]: Closing Board Control Port()
    [13:26:56]  [RadarAPI]: Status: Passed
    [13:26:56]  [RadarAPI]: ar1.PowerOff()
    [13:26:56]  [RadarAPI]: Status: Passed
    [13:26:57]  [RadarAPI]: Opening Gpio Control Port()
    [13:26:57]  [RadarAPI]: Status: Passed
    [13:26:58]  [RadarAPI]: Opening Board Control Port()
    [13:26:58]  [RadarAPI]: Status: Passed
    [13:26:59]  [RadarAPI]: ar1.FullReset()
    [13:26:59]  [RadarAPI]: Status: Passed
    [13:26:59]  [RadarAPI]: Closing Board Control Port()
    [13:26:59]  [RadarAPI]: Status: Passed
    [13:26:59]  [RadarAPI]: Closing Gpio Control Port()
    [13:26:59]  [RadarAPI]: Status: Passed
    [13:26:59]  [RadarAPI]: ar1.SOPControl(2)
    [13:26:59]  [RadarAPI]: Status: Passed
    [13:26:59]  [RadarAPI]: ar1.Connect(14,921600,1000)
    [13:27:02]  [RadarAPI]: Warning: Connected with baudrate 115200
    [13:27:03]  [RadarAPI]: Warning: Disconnected existing BaudRate
    [13:27:04]  [RadarAPI]: Warning: Trying to connect with baudrate 921600
    [13:27:05]  [RadarAPI]: ar1.Calling_IsConnected()
    [13:27:06]  [RadarAPI]: Part number of the device = 0x98
    [13:27:06]  [RadarAPI]: Device type = GP
    [13:27:06]  [RadarAPI]: ar1.SelectChipVersion("AWR2944")
    [13:27:06]  [RadarAPI]: Status: Passed
    [13:27:06]  Device Status : AWR2944/GP/ASIL-B/SOP:2/ES:2.0
    [13:27:06]  [RadarAPI]: ar1.Calling_IsConnected()
    [13:27:07]  [RadarAPI]: Part number of the device = 0x98
    [13:27:07]  [RadarAPI]: Device type = GP
    [13:27:07]  [RadarAPI]: ar1.SelectChipVersion("AWR2944")
    [13:27:08]  [RadarAPI]: Status: Passed
    [13:27:08]  Device Status : AWR2944/GP/ASIL-B/SOP:2/ES:2.0
    [13:27:08]  [RadarAPI]: ar1.SelectChipVersion("AR1642")
    [13:27:08]  [RadarAPI]: Status: Passed
    [13:27:08]  [RadarAPI]: ar1.frequencyBandSelection("77G")
    [13:27:08]  [RadarAPI]: ar1.SelectChipVersion("AR1642")
    [13:27:08]  [RadarAPI]: Status: Passed
    [13:27:08]  [RadarAPI]: ar1.DownloadBSSFw("F:\\ti\\mmwave_studio_03_01_03_01\\rf_eval_firmware\\radarss\\xwr29xx_radarss_rprc.bin")
    [13:27:12]  [RadarAPI]: ar1.GetBSSFwVersion()
    [13:27:12]  [RadarAPI]: BSSFwVersion:(02.04.05.03 (20/04/22))
    [13:27:12]  [RadarAPI]: ar1.GetBSSPatchFwVersion()
    [13:27:12]  [RadarAPI]: BSSPatchFwVersion:(02.04.09.05 (28/06/23))
    [13:27:13]  [RadarAPI]: ar1.DownloadMSSFw("F:\\ti\\mmwave_studio_03_01_03_01\\rf_eval_firmware\\masterss\\xwr2xxx_masterss.bin")
    [13:27:16]  [RadarAPI]: Downloading MSS RPRC Binary..
    [13:27:20]  [RadarAPI]: ar1.GetMSSFwVersion()
    [13:27:20]  [RadarAPI]: MSSFwVersion:(02.04.02.12 (05/01/24))
    [13:27:21]  MSS power up done async event received!
    [13:27:21]  [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0)
    [13:27:21]  [RadarAPI]: Status: Passed
    [13:27:21]  [RadarAPI]: ar1.RfEnable()
    [13:27:21]  BSS power up done async event received!
    [13:27:21]  [RadarAPI]: Status: Passed
    [13:27:22]  [RadarAPI]: ar1.GetMSSFwVersion()
    [13:27:22]  [RadarAPI]: MSSFwVersion:(02.04.02.12 (05/01/24))
    [13:27:22]  [RadarAPI]: ar1.GetBSSFwVersion()
    [13:27:22]  [RadarAPI]: BSSFwVersion:(02.04.05.03 (20/04/22))
    [13:27:23]  [RadarAPI]: ar1.GetBSSPatchFwVersion()
    [13:27:23]  [RadarAPI]: BSSPatchFwVersion:(02.04.09.05 (28/06/23))
    [13:27:24]  [RadarAPI]: ar1.ChanNAdcConfig(1, 1, 0, 0, 1, 1, 1, 1, 2, 0, 0)
    [13:27:24]  [RadarAPI]: Status: Passed
    [13:27:24]  [RadarAPI]: ar1.LPModConfig(0, 0)
    [13:27:24]  [RadarAPI]: Status: Passed
    [13:27:24]  [RadarAPI]: ar1.RfInit()
    [13:27:24]  RF Init async event received!
    [13:27:24]  [RadarAPI]: Time stamp, Temperture: 3054,41; SynthVCO3 Status, Update: 0, 0; APLL Status, Update: 1, 0; SynthVCO1 Status, Update: 1, 1; SynthVCO2 Status, Update: 1, 1; LODist Status, Update: 1, 1; RxADCDC Status, Update: 1, 1; HPFcutoff Status, Update: 1, 1; LPFcutoff Status, Update: 1, 1; PeakDetector Status, Update: 1, 1; TxPower Status, Update: 1, 1; RxGain Status, Update: 1, 1; TxPhase Status, Update: 1, 1; RxIQMM Status, Update: 0, 0; 
    [13:27:24]  [RadarAPI]: Status: Passed
    [13:27:24]  [RadarAPI]: ar1.DataPathConfig(513, 1216644097, 0)
    [13:27:24]  [RadarAPI]: Status: Passed
    [13:27:24]  [RadarAPI]: ar1.LVDSLaneConfig(0, 1, 1, 0, 0, 1, 0, 0)
    [13:27:24]  [RadarAPI]: Status: Passed
    [13:27:24]  [RadarAPI]: ar1.SetTestSource(4, 3, 0, 0, 0, 0, -327, 0, -327, 327, 327, 327, -2.5, 327, 327, 0, 0, 0, 0, -327, 0, -327, 327, 327, 327, -95, 0, 0, 0.5, 0, 1, 0, 1.5, 0, 0, 0, 0, 0, 0, 0, 0)
    [13:27:24]  [RadarAPI]: Status: Passed
    [13:27:24]  [RadarAPI]: ar1.ProfileConfig(0, 80.000000006, 6, 4, 20, 0, 0, 0, 0, 0, 0, 0, 0, 3.042, 0, 256, 17000, 2216755200, 0, 158, 0, 0, 0)
    [13:27:25]  [RadarAPI]: Status: Passed
    [13:27:25]  [RadarAPI]: ar1.ChirpConfig(0, 0, 0, 0, 0, 0, 0, 1, 0, 0, 0)
    [13:27:25]  [RadarAPI]: Status: Passed
    [13:27:25]  Test Source Already Enabled...!!!
    [13:27:25]  [RadarAPI]: ar1.DisableTestSource(0)
    [13:27:25]  [RadarAPI]: Status: Passed
    [13:27:25]  [RadarAPI]: ar1.AdvanceFrameConfig(4, 1536, 0, 0, 1, 255, 1600000, 0, 1, 3, 5000000, 0, 0, 1, 255, 1600000, 0,1, 3, 5000000, 0, 0, 1, 255, 1600000, 0, 1, 3, 5000000, 0, 0, 1, 255,1600000, 0, 1, 3, 5000000, 64, 1, 0, 4, 765, 256, 1, 765, 256, 1, 765,256, 1, 765, 256, 1)
    [13:27:25]  [RadarAPI]: Status: Passed
    [13:27:25]  [RadarAPI]: ar1.GetCaptureCardDllVersion()
    [13:27:25]  [RadarAPI]: Sending dll_version command to DCA1000
    [13:27:25]  [RadarAPI]: 
    [13:27:25]  DLL Version : 1.0
    [13:27:25]  [RadarAPI]: ar1.SelectCaptureDevice("DCA1000")
    [13:27:25]  [RadarAPI]: Status: Passed
    [13:27:25]  [RadarAPI]: ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "c:22:38:4e:5a:c", 4096, 4098)
    [13:27:25]  [RadarAPI]: Sending fpga command to DCA1000
    [13:27:25]  [RadarAPI]: 
    [13:27:25]  
    [13:27:25]  
    [13:27:25]  ConfigureRFDCCard_Mode(): UDP write failed : 10051
    [13:27:25]  FPGA Configuration : 
    [13:27:25]  Sending command failed - -3
    [13:27:25]  [RadarAPI]: Sending fpga_version command to DCA1000
    [13:27:25]  [RadarAPI]: 
    [13:27:25]  
    [13:27:25]  
    [13:27:25]  ReadRFDCCard_FpgaVersion(): UDP write failed : 10051
    [13:27:25]  
    [13:27:25]  [RadarAPI]: ar1.CaptureCardConfig_Mode(1, 2, 1, 2, 3, 0)
    [13:27:25]  [RadarAPI]: Sending fpga command to DCA1000
    [13:27:25]  [RadarAPI]: 
    [13:27:25]  
    [13:27:25]  
    [13:27:25]  ConfigureRFDCCard_Mode(): UDP write failed : 10051
    [13:27:25]  FPGA Configuration : 
    [13:27:25]  Sending command failed - -3
    [13:27:25]  [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25)
    [13:27:25]  [RadarAPI]: Sending fpga command to DCA1000
    [13:27:25]  [RadarAPI]: 
    [13:27:25]  
    [13:27:25]  
    [13:27:25]  ConfigureRFDCCard_Mode(): UDP write failed : 10051
    [13:27:25]  FPGA Configuration : 
    [13:27:25]  Sending command failed - -3
    [13:27:25]  [RadarAPI]: Sending record command to DCA1000
    [13:27:25]  [RadarAPI]: 
    [13:27:25]  
    [13:27:25]  
    [13:27:25]  ConfigureRFDCCard_Record(): UDP write failed : 10051
    [13:27:25]  Configure Record : 
    [13:27:25]  Sending command failed - -3
    [13:27:25]  [RadarAPI]: ar1.GetCaptureCardFPGAVersion()
    [13:27:25]  [RadarAPI]: Sending fpga_version command to DCA1000
    [13:27:26]  [RadarAPI]: 
    [13:27:26]  
    [13:27:26]  
    [13:27:26]  ReadRFDCCard_FpgaVersion(): UDP write failed : 10051
    [13:27:26]  
    [13:27:26]  [RadarAPI]: ar1.CaptureCardConfig_StartRecord("F:\\ti\\mmwave_studio_03_01_03_01\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
    [13:27:26]  [RadarAPI]: Sending start_record command to DCA1000
    [13:27:26]  [RadarAPI]: Status: Passed
    [13:27:26]  RSTD.ShowLogFile()
    [13:27:26]  
    [13:27:26]  ***Script completed successfully.***
    [13:27:41]  [RadarAPI]: ar1.CaptureCardConfig_StartRecord("F:\\ti\\mmwave_studio_03_01_03_01\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
    [13:27:41]  [RadarAPI]: Sending start_record command to DCA1000
    [13:27:41]  [RadarAPI]: 
    [13:27:41]  
    [13:27:41]  
    [13:27:41]  StartRecordData(): UDP write failed : 10051
    [13:27:41]  Start Record : 
    [13:27:41]  Sending command failed - -3
    [13:28:20]  LuaLoad("F:/dns_liliang/LUAScript/new_DataCapture_2944_test.lua")
    [13:28:20]  [RadarAPI]: ar1.Disconnect()
    [13:28:20]  [RadarAPI]: ar1.Calling_ATE_DisconnectTarget()
    [13:28:20]  [RadarAPI]: ar1.Calling_IsConnected()
    [13:28:20]  [RadarAPI]: ar1.SaveSettings('C:\Users\Administrator\AppData\Roaming\RSTD\ar1gui.ini')
    [13:28:20]  [RadarAPI]: Opening Board Control Port()
    [13:28:20]  [RadarAPI]: Status: Passed
    [13:28:21]  [RadarAPI]: ar1.FullReset()
    [13:28:21]  [RadarAPI]: Status: Passed
    [13:28:22]  [RadarAPI]: Closing Board Control Port()
    [13:28:22]  [RadarAPI]: Status: Passed
    [13:28:22]  [RadarAPI]: ar1.PowerOff()
    [13:28:22]  [RadarAPI]: Status: Passed
    [13:28:23]  [RadarAPI]: Opening Gpio Control Port()
    [13:28:23]  [RadarAPI]: Status: Passed
    [13:28:23]  [RadarAPI]: Opening Board Control Port()
    [13:28:23]  [RadarAPI]: Status: Passed
    [13:28:24]  [RadarAPI]: ar1.FullReset()
    [13:28:24]  [RadarAPI]: Status: Passed
    [13:28:25]  [RadarAPI]: Closing Board Control Port()
    [13:28:25]  [RadarAPI]: Status: Passed
    [13:28:25]  [RadarAPI]: Closing Gpio Control Port()
    [13:28:25]  [RadarAPI]: Status: Passed
    [13:28:25]  [RadarAPI]: ar1.SOPControl(2)
    [13:28:25]  [RadarAPI]: Status: Passed
    [13:28:25]  [RadarAPI]: ar1.Connect(14,921600,1000)
    [13:28:28]  [RadarAPI]: Warning: Connected with baudrate 115200
    [13:28:29]  [RadarAPI]: Warning: Disconnected existing BaudRate
    [13:28:29]  [RadarAPI]: Warning: Trying to connect with baudrate 921600
    [13:28:30]  [RadarAPI]: ar1.Calling_IsConnected()
    [13:28:32]  [RadarAPI]: Part number of the device = 0x98
    [13:28:32]  [RadarAPI]: Device type = GP
    [13:28:32]  [RadarAPI]: ar1.SelectChipVersion("AWR2944")
    [13:28:32]  [RadarAPI]: Status: Passed
    [13:28:32]  Device Status : AWR2944/GP/ASIL-B/SOP:2/ES:2.0
    [13:28:32]  [RadarAPI]: ar1.Calling_IsConnected()
    [13:28:33]  [RadarAPI]: Part number of the device = 0x98
    [13:28:33]  [RadarAPI]: Device type = GP
    [13:28:33]  [RadarAPI]: ar1.SelectChipVersion("AWR2944")
    [13:28:33]  [RadarAPI]: Status: Passed
    [13:28:33]  Device Status : AWR2944/GP/ASIL-B/SOP:2/ES:2.0
    [13:28:33]  [RadarAPI]: ar1.SelectChipVersion("AR1642")
    [13:28:33]  [RadarAPI]: Status: Passed
    [13:28:33]  [RadarAPI]: ar1.frequencyBandSelection("77G")
    [13:28:33]  [RadarAPI]: ar1.SelectChipVersion("AR1642")
    [13:28:33]  [RadarAPI]: Status: Passed
    [13:28:33]  [RadarAPI]: ar1.DownloadBSSFw("F:\\ti\\mmwave_studio_03_01_03_01\\rf_eval_firmware\\radarss\\xwr29xx_radarss_rprc.bin")
    [13:28:37]  [RadarAPI]: ar1.GetBSSFwVersion()
    [13:28:37]  [RadarAPI]: BSSFwVersion:(02.04.05.03 (20/04/22))
    [13:28:38]  [RadarAPI]: ar1.GetBSSPatchFwVersion()
    [13:28:38]  [RadarAPI]: BSSPatchFwVersion:(02.04.09.05 (28/06/23))
    [13:28:39]  [RadarAPI]: ar1.DownloadMSSFw("F:\\ti\\mmwave_studio_03_01_03_01\\rf_eval_firmware\\masterss\\xwr2xxx_masterss.bin")
    [13:28:41]  [RadarAPI]: Downloading MSS RPRC Binary..
    [13:28:46]  [RadarAPI]: ar1.GetMSSFwVersion()
    [13:28:46]  [RadarAPI]: MSSFwVersion:(02.04.02.12 (05/01/24))
    [13:28:46]  MSS power up done async event received!
    [13:28:46]  [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0)
    [13:28:46]  [RadarAPI]: Status: Passed
    [13:28:46]  [RadarAPI]: ar1.RfEnable()
    [13:28:47]  BSS power up done async event received!
    [13:28:47]  [RadarAPI]: Status: Passed
    [13:28:47]  [RadarAPI]: ar1.GetMSSFwVersion()
    [13:28:47]  [RadarAPI]: MSSFwVersion:(02.04.02.12 (05/01/24))
    [13:28:47]  [RadarAPI]: ar1.GetBSSFwVersion()
    [13:28:47]  [RadarAPI]: BSSFwVersion:(02.04.05.03 (20/04/22))
    [13:28:48]  [RadarAPI]: ar1.GetBSSPatchFwVersion()
    [13:28:48]  [RadarAPI]: BSSPatchFwVersion:(02.04.09.05 (28/06/23))
    [13:28:49]  [RadarAPI]: ar1.ChanNAdcConfig(1, 1, 0, 0, 1, 1, 1, 1, 2, 0, 0)
    [13:28:49]  [RadarAPI]: Status: Passed
    [13:28:49]  [RadarAPI]: ar1.LPModConfig(0, 0)
    [13:28:50]  [RadarAPI]: Status: Passed
    [13:28:50]  [RadarAPI]: ar1.RfInit()
    [13:28:50]  RF Init async event received!
    [13:28:50]  [RadarAPI]: Time stamp, Temperture: 3049,41; SynthVCO3 Status, Update: 0, 0; APLL Status, Update: 1, 0; SynthVCO1 Status, Update: 1, 1; SynthVCO2 Status, Update: 1, 1; LODist Status, Update: 1, 1; RxADCDC Status, Update: 1, 1; HPFcutoff Status, Update: 1, 1; LPFcutoff Status, Update: 1, 1; PeakDetector Status, Update: 1, 1; TxPower Status, Update: 1, 1; RxGain Status, Update: 1, 1; TxPhase Status, Update: 1, 1; RxIQMM Status, Update: 0, 0; 
    [13:28:50]  [RadarAPI]: Status: Passed
    [13:28:50]  [RadarAPI]: ar1.DataPathConfig(513, 1216644097, 0)
    [13:28:50]  [RadarAPI]: Status: Passed
    [13:28:50]  [RadarAPI]: ar1.LVDSLaneConfig(0, 1, 1, 0, 0, 1, 0, 0)
    [13:28:50]  [RadarAPI]: Status: Passed
    [13:28:50]  [RadarAPI]: ar1.SetTestSource(4, 3, 0, 0, 0, 0, -327, 0, -327, 327, 327, 327, -2.5, 327, 327, 0, 0, 0, 0, -327, 0, -327, 327, 327, 327, -95, 0, 0, 0.5, 0, 1, 0, 1.5, 0, 0, 0, 0, 0, 0, 0, 0)
    [13:28:50]  [RadarAPI]: Status: Passed
    [13:28:50]  [RadarAPI]: ar1.ProfileConfig(0, 80.000000006, 6, 4, 20, 0, 0, 0, 0, 0, 0, 0, 0, 3.042, 0, 256, 17000, 2216755200, 0, 158, 0, 0, 0)
    [13:28:50]  [RadarAPI]: Status: Passed
    [13:28:50]  [RadarAPI]: ar1.ChirpConfig(0, 0, 0, 0, 0, 0, 0, 1, 0, 0, 0)
    [13:28:50]  [RadarAPI]: Status: Passed
    [13:28:50]  Test Source Already Enabled...!!!
    [13:28:50]  [RadarAPI]: ar1.DisableTestSource(0)
    [13:28:50]  [RadarAPI]: Status: Passed
    [13:28:50]  [RadarAPI]: ar1.AdvanceFrameConfig(4, 1536, 0, 0, 1, 255, 1600000, 0, 1, 3, 5000000, 0, 0, 1, 255, 1600000, 0,1, 3, 5000000, 0, 0, 1, 255, 1600000, 0, 1, 3, 5000000, 0, 0, 1, 255,1600000, 0, 1, 3, 5000000, 64, 1, 0, 4, 765, 256, 1, 765, 256, 1, 765,256, 1, 765, 256, 1)
    [13:28:50]  [RadarAPI]: Status: Passed
    [13:28:50]  [RadarAPI]: ar1.GetCaptureCardDllVersion()
    [13:28:50]  [RadarAPI]: Sending dll_version command to DCA1000
    [13:28:50]  [RadarAPI]: 
    [13:28:50]  DLL Version : 1.0
    [13:28:50]  [RadarAPI]: ar1.SelectCaptureDevice("DCA1000")
    [13:28:50]  [RadarAPI]: Status: Passed
    [13:28:50]  [RadarAPI]: ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "c:22:38:4e:5a:c", 4096, 4098)
    [13:28:50]  [RadarAPI]: Sending fpga command to DCA1000
    [13:28:50]  [RadarAPI]: 
    [13:28:50]  
    [13:28:50]  
    [13:28:50]  ConfigureRFDCCard_Mode(): UDP write failed : 10051
    [13:28:50]  FPGA Configuration : 
    [13:28:50]  Sending command failed - -3
    [13:28:50]  [RadarAPI]: Sending fpga_version command to DCA1000
    [13:28:50]  [RadarAPI]: 
    [13:28:50]  
    [13:28:50]  
    [13:28:50]  ReadRFDCCard_FpgaVersion(): UDP write failed : 10051
    [13:28:50]  
    [13:28:50]  [RadarAPI]: ar1.CaptureCardConfig_Mode(1, 2, 1, 2, 3, 0)
    [13:28:50]  [RadarAPI]: Sending fpga command to DCA1000
    [13:28:51]  [RadarAPI]: 
    [13:28:51]  
    [13:28:51]  
    [13:28:51]  ConfigureRFDCCard_Mode(): UDP write failed : 10051
    [13:28:51]  FPGA Configuration : 
    [13:28:51]  Sending command failed - -3
    [13:28:51]  [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25)
    [13:28:51]  [RadarAPI]: Sending fpga command to DCA1000
    [13:28:51]  [RadarAPI]: 
    [13:28:51]  
    [13:28:51]  
    [13:28:51]  ConfigureRFDCCard_Mode(): UDP write failed : 10051
    [13:28:51]  FPGA Configuration : 
    [13:28:51]  Sending command failed - -3
    [13:28:51]  [RadarAPI]: Sending record command to DCA1000
    [13:28:51]  [RadarAPI]: 
    [13:28:51]  
    [13:28:51]  
    [13:28:51]  ConfigureRFDCCard_Record(): UDP write failed : 10051
    [13:28:51]  Configure Record : 
    [13:28:51]  Sending command failed - -3
    [13:28:51]  [RadarAPI]: ar1.GetCaptureCardFPGAVersion()
    [13:28:51]  [RadarAPI]: Sending fpga_version command to DCA1000
    [13:28:51]  [RadarAPI]: 
    [13:28:51]  
    [13:28:51]  
    [13:28:51]  ReadRFDCCard_FpgaVersion(): UDP write failed : 10051
    [13:28:51]  
    [13:28:51]  [RadarAPI]: ar1.CaptureCardConfig_StartRecord("F:\\ti\\mmwave_studio_03_01_03_01\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
    [13:28:51]  [RadarAPI]: Sending start_record command to DCA1000
    [13:28:51]  [RadarAPI]: Status: Passed
    [13:28:51]  RSTD.ShowLogFile()
    [13:28:51]  
    [13:28:51]  ***Script completed successfully.***
    [13:29:02]  [RadarAPI]: ar1.CaptureCardConfig_StartRecord("F:\\ti\\mmwave_studio_03_01_03_01\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
    [13:29:02]  [RadarAPI]: Sending start_record command to DCA1000
    [13:29:03]  [RadarAPI]: 
    [13:29:03]  
    [13:29:03]  
    [13:29:03]  StartRecordData(): UDP write failed : 10051
    [13:29:03]  Start Record : 
    [13:29:03]  Sending command failed - -3
    [13:29:10]  [RadarAPI]: ar1.GetCaptureCardDllVersion()
    [13:29:10]  [RadarAPI]: Sending dll_version command to DCA1000
    [13:29:10]  [RadarAPI]: 
    [13:29:10]  DLL Version : 1.0
    [13:29:10]  [RadarAPI]: ar1.SelectCaptureDevice("DCA1000")
    [13:29:10]  [RadarAPI]: Status: Passed
    [13:29:16]  [RadarAPI]: ar1.CaptureCardConfig_StartRecord("F:\\ti\\mmwave_studio_03_01_03_01\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
    [13:29:16]  [RadarAPI]: Sending start_record command to DCA1000
    [13:29:16]  [RadarAPI]: 
    [13:29:16]  
    [13:29:16]  
    [13:29:16]  StartRecordData(): UDP write failed : 10051
    [13:29:16]  Start Record : 
    [13:29:16]  Sending command failed - -3
    [13:29:20]  [RadarAPI]: ar1.StartFrame()
    [13:29:20]  [RadarAPI]: Status: Hardware select :GlobalRef.g_TriggerSelectSW_HW value: False
    [13:29:20]  [RadarAPI]: Status: Passed
    [13:29:20]  Frame start async event received!
    [13:29:26]  Frame End async event received!
    [13:29:26]  [RadarAPI]: Frame Ended
    [13:29:32]  [RadarAPI]: ar1.CaptureCardConfig_StartRecord("F:\\ti\\mmwave_studio_03_01_03_01\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
    [13:29:32]  [RadarAPI]: Sending start_record command to DCA1000
    [13:29:32]  [RadarAPI]: 
    [13:29:32]  
    [13:29:32]  
    [13:29:32]  StartRecordData(): UDP write failed : 10051
    [13:29:32]  Start Record : 
    [13:29:32]  Sending command failed - -3
    [13:29:56]  [RadarAPI]: ar1.CaptureCardConfig_StartRecord("F:\\ti\\mmwave_studio_03_01_03_01\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
    [13:29:56]  [RadarAPI]: Sending start_record command to DCA1000
    [13:30:16]  [RadarAPI]: ar1.StartFrame()
    [13:30:16]  [RadarAPI]: Status: Hardware select :GlobalRef.g_TriggerSelectSW_HW value: False
    [13:30:16]  [RadarAPI]: Status: Passed
    [13:30:16]  Frame start async event received!
    [13:30:22]  Frame End async event received!
    [13:30:22]  [RadarAPI]: Frame Ended
    [13:30:25]  [RadarAPI]: 
    [13:30:25]  [RadarAPI]: 
    [13:30:25]  Start Record command : Success
    [13:30:25]  
    [13:30:25]  No LVDS data
    [13:30:25]  
    [13:30:25]  No Header
    [13:30:25]  
    [13:30:25]  Record stop is done successfully
    [13:30:27]  [RadarAPI]: ar1.StartMatlabPostProc("F:\\ti\\mmwave_studio_03_01_03_01\\mmWaveStudio\\PostProc\\adc_data.bin")
    [13:30:27]  [RadarAPI]: No of files Captured: 1, Total no of frames for each device : 64
    [13:31:05]  [RadarAPI]: ar1.CaptureCardConfig_StartRecord("F:\\ti\\mmwave_studio_03_01_03_01\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
    [13:31:05]  [RadarAPI]: Sending start_record command to DCA1000
    [13:31:10]  [RadarAPI]: ar1.StartFrame()
    [13:31:10]  [RadarAPI]: Status: Hardware select :GlobalRef.g_TriggerSelectSW_HW value: False
    [13:31:10]  [RadarAPI]: Status: Passed
    [13:31:10]  Frame start async event received!
    [13:31:16]  Frame End async event received!
    [13:31:16]  [RadarAPI]: Frame Ended
    [13:31:34]  [RadarAPI]: 
    [13:31:34]  [RadarAPI]: 
    [13:31:34]  Start Record command : Success
    [13:31:34]  
    [13:31:34]  No LVDS data
    [13:31:34]  
    [13:31:34]  No Header
    [13:31:34]  
    [13:31:34]  Record stop is done successfully
    [13:31:34]  [RadarAPI]: ar1.StartMatlabPostProc("F:\\ti\\mmwave_studio_03_01_03_01\\mmWaveStudio\\PostProc\\adc_data.bin")
    [13:31:34]  [RadarAPI]: No of files Captured: 1, Total no of frames for each device : 64
    [13:32:25]  LuaLoad("F:/dns_liliang/LUAScript/new_DataCapture_2944_test.lua")
    [13:32:25]  [RadarAPI]: ar1.Disconnect()
    [13:32:25]  [RadarAPI]: ar1.Calling_ATE_DisconnectTarget()
    [13:32:25]  [RadarAPI]: ar1.Calling_IsConnected()
    [13:32:25]  [RadarAPI]: ar1.SaveSettings('C:\Users\Administrator\AppData\Roaming\RSTD\ar1gui.ini')
    [13:32:26]  [RadarAPI]: Opening Board Control Port()
    [13:32:26]  [RadarAPI]: Status: Passed
    [13:32:27]  [RadarAPI]: ar1.FullReset()
    [13:32:27]  [RadarAPI]: Status: Passed
    [13:32:28]  [RadarAPI]: Closing Board Control Port()
    [13:32:28]  [RadarAPI]: Status: Passed
    [13:32:28]  [RadarAPI]: ar1.PowerOff()
    [13:32:28]  [RadarAPI]: Status: Passed
    [13:32:28]  [RadarAPI]: Opening Gpio Control Port()
    [13:32:28]  [RadarAPI]: Status: Passed
    [13:32:29]  [RadarAPI]: Opening Board Control Port()
    [13:32:29]  [RadarAPI]: Status: Passed
    [13:32:30]  [RadarAPI]: ar1.FullReset()
    [13:32:30]  [RadarAPI]: Status: Passed
    [13:32:30]  [RadarAPI]: Closing Board Control Port()
    [13:32:30]  [RadarAPI]: Status: Passed
    [13:32:31]  [RadarAPI]: Closing Gpio Control Port()
    [13:32:31]  [RadarAPI]: Status: Passed
    [13:32:31]  [RadarAPI]: ar1.SOPControl(2)
    [13:32:31]  [RadarAPI]: Status: Passed
    [13:32:31]  [RadarAPI]: ar1.Connect(14,921600,1000)
    [13:32:33]  [RadarAPI]: Warning: Connected with baudrate 115200
    [13:32:34]  [RadarAPI]: Warning: Disconnected existing BaudRate
    [13:32:35]  [RadarAPI]: Warning: Trying to connect with baudrate 921600
    [13:32:36]  [RadarAPI]: ar1.Calling_IsConnected()
    [13:32:37]  [RadarAPI]: Part number of the device = 0x98
    [13:32:37]  [RadarAPI]: Device type = GP
    [13:32:37]  [RadarAPI]: ar1.SelectChipVersion("AWR2944")
    [13:32:37]  [RadarAPI]: Status: Passed
    [13:32:37]  Device Status : AWR2944/GP/ASIL-B/SOP:2/ES:2.0
    [13:32:37]  [RadarAPI]: ar1.Calling_IsConnected()
    [13:32:39]  [RadarAPI]: Part number of the device = 0x98
    [13:32:39]  [RadarAPI]: Device type = GP
    [13:32:39]  [RadarAPI]: ar1.SelectChipVersion("AWR2944")
    [13:32:39]  [RadarAPI]: Status: Passed
    [13:32:39]  Device Status : AWR2944/GP/ASIL-B/SOP:2/ES:2.0
    [13:32:39]  [RadarAPI]: ar1.SelectChipVersion("AR1642")
    [13:32:39]  [RadarAPI]: Status: Passed
    [13:32:39]  [RadarAPI]: ar1.frequencyBandSelection("77G")
    [13:32:39]  [RadarAPI]: ar1.SelectChipVersion("AR1642")
    [13:32:39]  [RadarAPI]: Status: Passed
    [13:32:39]  [RadarAPI]: ar1.DownloadBSSFw("F:\\ti\\mmwave_studio_03_01_03_01\\rf_eval_firmware\\radarss\\xwr29xx_radarss_rprc.bin")
    [13:32:43]  [RadarAPI]: ar1.GetBSSFwVersion()
    [13:32:43]  [RadarAPI]: BSSFwVersion:(02.04.05.03 (20/04/22))
    [13:32:44]  [RadarAPI]: ar1.GetBSSPatchFwVersion()
    [13:32:44]  [RadarAPI]: BSSPatchFwVersion:(02.04.09.05 (28/06/23))
    [13:32:44]  [RadarAPI]: ar1.DownloadMSSFw("F:\\ti\\mmwave_studio_03_01_03_01\\rf_eval_firmware\\masterss\\xwr2xxx_masterss.bin")
    [13:32:47]  [RadarAPI]: Downloading MSS RPRC Binary..
    [13:32:51]  [RadarAPI]: ar1.GetMSSFwVersion()
    [13:32:51]  [RadarAPI]: MSSFwVersion:(02.04.02.12 (05/01/24))
    [13:32:52]  MSS power up done async event received!
    [13:32:52]  [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0)
    [13:32:52]  [RadarAPI]: Status: Passed
    [13:32:52]  [RadarAPI]: ar1.RfEnable()
    [13:32:52]  BSS power up done async event received!
    [13:32:52]  [RadarAPI]: Status: Passed
    [13:32:53]  [RadarAPI]: ar1.GetMSSFwVersion()
    [13:32:53]  [RadarAPI]: MSSFwVersion:(02.04.02.12 (05/01/24))
    [13:32:53]  [RadarAPI]: ar1.GetBSSFwVersion()
    [13:32:53]  [RadarAPI]: BSSFwVersion:(02.04.05.03 (20/04/22))
    [13:32:54]  [RadarAPI]: ar1.GetBSSPatchFwVersion()
    [13:32:54]  [RadarAPI]: BSSPatchFwVersion:(02.04.09.05 (28/06/23))
    [13:32:55]  [RadarAPI]: ar1.ChanNAdcConfig(1, 1, 0, 0, 1, 1, 1, 1, 2, 0, 0)
    [13:32:55]  [RadarAPI]: Status: Passed
    [13:32:55]  [RadarAPI]: ar1.LPModConfig(0, 0)
    [13:32:55]  [RadarAPI]: Status: Passed
    [13:32:55]  [RadarAPI]: ar1.RfInit()
    [13:32:55]  RF Init async event received!
    [13:32:55]  [RadarAPI]: Time stamp, Temperture: 3042,42; SynthVCO3 Status, Update: 0, 0; APLL Status, Update: 1, 0; SynthVCO1 Status, Update: 1, 1; SynthVCO2 Status, Update: 1, 1; LODist Status, Update: 1, 1; RxADCDC Status, Update: 1, 1; HPFcutoff Status, Update: 1, 1; LPFcutoff Status, Update: 1, 1; PeakDetector Status, Update: 1, 1; TxPower Status, Update: 1, 1; RxGain Status, Update: 1, 1; TxPhase Status, Update: 1, 1; RxIQMM Status, Update: 0, 0; 
    [13:32:55]  [RadarAPI]: Status: Passed
    [13:32:55]  [RadarAPI]: ar1.DataPathConfig(513, 1216644097, 0)
    [13:32:55]  [RadarAPI]: Status: Passed
    [13:32:55]  [RadarAPI]: ar1.LVDSLaneConfig(0, 1, 1, 0, 0, 1, 0, 0)
    [13:32:56]  [RadarAPI]: Status: Passed
    [13:32:56]  [RadarAPI]: ar1.SetTestSource(4, 3, 0, 0, 0, 0, -327, 0, -327, 327, 327, 327, -2.5, 327, 327, 0, 0, 0, 0, -327, 0, -327, 327, 327, 327, -95, 0, 0, 0.5, 0, 1, 0, 1.5, 0, 0, 0, 0, 0, 0, 0, 0)
    [13:32:56]  [RadarAPI]: Status: Passed
    [13:32:56]  [RadarAPI]: ar1.ProfileConfig(0, 80.000000006, 6, 4, 20, 0, 0, 0, 0, 0, 0, 0, 0, 3.042, 0, 256, 17000, 2216755200, 0, 158, 0, 0, 0)
    [13:32:56]  [RadarAPI]: Status: Passed
    [13:32:56]  [RadarAPI]: ar1.ChirpConfig(0, 0, 0, 0, 0, 0, 0, 1, 0, 0, 0)
    [13:32:56]  [RadarAPI]: Status: Passed
    [13:32:56]  Test Source Already Enabled...!!!
    [13:32:56]  [RadarAPI]: ar1.DisableTestSource(0)
    [13:32:56]  [RadarAPI]: Status: Passed
    [13:32:56]  [RadarAPI]: ar1.AdvanceFrameConfig(4, 1536, 0, 0, 1, 255, 1600000, 0, 1, 3, 5000000, 0, 0, 1, 255, 1600000, 0,1, 3, 5000000, 0, 0, 1, 255, 1600000, 0, 1, 3, 5000000, 0, 0, 1, 255,1600000, 0, 1, 3, 5000000, 64, 1, 0, 4, 765, 256, 1, 765, 256, 1, 765,256, 1, 765, 256, 1)
    [13:32:56]  [RadarAPI]: Status: Passed
    [13:32:56]  [RadarAPI]: ar1.GetCaptureCardDllVersion()
    [13:32:56]  [RadarAPI]: Sending dll_version command to DCA1000
    [13:32:56]  [RadarAPI]: 
    [13:32:56]  DLL Version : 1.0
    [13:32:56]  [RadarAPI]: ar1.SelectCaptureDevice("DCA1000")
    [13:32:56]  [RadarAPI]: Status: Passed
    [13:32:56]  [RadarAPI]: ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "c:22:38:4e:5a:c", 4096, 4098)
    [13:32:56]  [RadarAPI]: Sending fpga command to DCA1000
    [13:32:56]  [RadarAPI]: 
    [13:32:56]  FPGA Configuration command : Success
    [13:32:56]  [RadarAPI]: Sending fpga_version command to DCA1000
    [13:32:56]  [RadarAPI]: 
    [13:32:56]  
    [13:32:56]  FPGA Version : 2.9 [Record]
    [13:32:56]  
    [13:32:56]  [RadarAPI]: ar1.CaptureCardConfig_Mode(1, 2, 1, 2, 3, 0)
    [13:32:56]  [RadarAPI]: Sending fpga command to DCA1000
    [13:32:56]  [RadarAPI]: 
    [13:32:56]  FPGA Configuration command : Success
    [13:32:56]  [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25)
    [13:32:56]  [RadarAPI]: Sending fpga command to DCA1000
    [13:32:56]  [RadarAPI]: 
    [13:32:56]  FPGA Configuration command : Success
    [13:32:56]  [RadarAPI]: Sending record command to DCA1000
    [13:32:57]  [RadarAPI]: 
    [13:32:57]  Configure Record command : Success
    [13:32:57]  [RadarAPI]: ar1.GetCaptureCardFPGAVersion()
    [13:32:57]  [RadarAPI]: Sending fpga_version command to DCA1000
    [13:32:57]  [RadarAPI]: 
    [13:32:57]  
    [13:32:57]  FPGA Version : 2.9 [Record]
    [13:32:57]  
    [13:32:57]  [RadarAPI]: ar1.CaptureCardConfig_StartRecord("F:\\ti\\mmwave_studio_03_01_03_01\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
    [13:32:57]  [RadarAPI]: Sending start_record command to DCA1000
    [13:32:57]  [RadarAPI]: Status: Passed
    [13:32:57]  RSTD.ShowLogFile()
    [13:32:57]  
    [13:32:57]  ***Script completed successfully.***
    [13:33:40]  [RadarAPI]: ar1.CaptureCardConfig_StartRecord("F:\\ti\\mmwave_studio_03_01_03_01\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
    [13:33:40]  [RadarAPI]: Sending start_record command to DCA1000
    [13:34:02]  [RadarAPI]: ar1.StartFrame()
    [13:34:02]  [RadarAPI]: Status: Hardware select :GlobalRef.g_TriggerSelectSW_HW value: False
    [13:34:02]  [RadarAPI]: Status: Passed
    [13:34:02]  Frame start async event received!
    [13:34:09]  Frame End async event received!
    [13:34:09]  [RadarAPI]: Frame Ended
    [13:34:15]  [RadarAPI]: 
    [13:34:15]  [RadarAPI]: 
    [13:34:15]  Start Record command : Success
    [13:34:15]  
    [13:34:15]  Record is completed
    [13:34:15]  
    [13:34:15]  Record stop is done successfully
    [13:34:17]  [RadarAPI]: ar1.StartMatlabPostProc("F:\\ti\\mmwave_studio_03_01_03_01\\mmWaveStudio\\PostProc\\adc_data.bin")
    [13:34:17]  [RadarAPI]: No of files Captured: 1, Total no of frames for each device : 64
    [13:34:53]  RSTD.ShowLogFile()
    [13:35:35]  RSTD.ShowLogFile()
    

  • Hello,

    Sorry for the delay. I will reproduce this and get back to you this week.

    Regards,

    Adrian

  • sorry,can you tell what happend?