This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM95241: Pullup resistor value

Part Number: LM95241

Tool/software:

Hi,

I am calculating Pullup resistance based on this article but the values don't align well. Can you please check and confirm what I am missing out?

Rpmin = (Vcc-VoL)/IoL = 2.5-0.8/(10uA) = 170kohms

Rpmax = tr/(cb*0.8473) = 1us/(400pF*0.8473) = 3kohms

Vcc = 2.5V is considered since my resistor pullup voltage is 2.5V even though the IC's supply is 3.3V

VoL = 0.8V taken from Pg 6 VIN(0) value

IoL = corresponding Logical “0” Input Current

Cb = 400pF for std mode

tr = 1us based on SMBus Rise Time in Pg6

Thanks