This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP236:Is it okay to force DC1~3V to Vout?

Part Number: TMP236

Tool/software:

I made a product that has a protection circuit that operates when overheated.

However, in order to verify, I have to force the voltage to increase on VOUT of TMP236.
Is it okay to force DC1~3V to Vout using dc power?