Part Number: MMWCAS-DSP-EVM
Other Parts Discussed in Thread: DRA742, PCF8575, PMP
Tool/software:
I am currently working with the MMWCAS-DSP-EVM and am working through the steps in the cascade user guide. There comes a step where the user must download the TDA firmware image from https://www.ti.com/tool/MMWAVE-STUDIO and then flash it to the device However, when I flash the image to the dive and try to boot it, I get the following error:
U-Boot 2016.05-00018-g6bc25a5 (Aug 05 2019 - 14:43:03 +0530)
CPU : DRA752-GP ES2.0
Model: TI DRA742
Board: DRA74x Cascade EVM REV H.4
DRAM: 4 GiB
MMC: i2c_write: error waiting for data ACK (status=0x116)
pcf8575_i2c_write_le16 i2c write failed to addr 21
OMAP SD/MMC: 0, OMAP SD/MMC: 1
Card did not respond to voltage select!
*** Warning - MMC init failed, using default environment
Card did not respond to voltage select!
ERROR: invalid mmc device
Has anyone seen this error before?
Thanks,
Thomas