This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV5033:磁気センサICの紹介

Part Number: DRV5033
Other Parts Discussed in Thread: DRV5013

Tool/software:

TIの磁気センサICにおいて

磁気センサIC(panasonic DN6851 交番磁界 pullup内臓 SIP3pin)の 置き換え検討をしております。

まずは10個ほど評価して入手したいと考えております。

使用可能なICがあれば紹介していただければと思っております。

入手性(価格、納期)が分かりますでしょうか?

よろしくお願いします。

  • Hi,

    Thanks for posting your question to the Sensors forum and welcome to E2E.

    We do not have a direct replacement for the DN6851 as we do not have any Hall-effect latches with a built-in pull up resistor.

    The DRV5013 would be the closest alternative, specifically the DRV5013BCQLPG. The DRV5013BC Bop max and Brp min are ±18mT, whereas the DN6851 Bop max and Brp min are ±30mT. The DRV5013 requires an external pullup resistor on the open-drain OUT pin. There also appear to be some slight differences in package dimensions.

    Please see the DRV5013 product page and datasheet linked here:

    Best regards,

    Jesse

  • こんにちは

    参考の上部品選定を行います。

    回答ありがとうございました。

    harada