Tool/software:
I have a IWR6843ISK along with DCA1000 and Boost board. I need to do an external hardware trigger. I have put in the required resistor on the boost board and hooked up a pulse generator (single shot) for the trigger into the J5 -9 on the boost board. I used mmWave Studio for the setup . I can get the board to trigger, but the internal matlab analysis firmware gives an error so I can't retrieve any data. It says the number of expected data points is slightly lower than expected. No matter what I have tried so far, this is always the case. The actual number is given in the errors I see. I can just switch over to firmware trigger, and it works fine. Back to hardware trigger, same error. Please help!
/Larry