This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWRL6432BOOST: CFG for people tracking with ceil-mount scenario

Part Number: IWRL6432BOOST


Tool/software:

Hi,

I am testing IWRL6432BOOST people tracking demo with ceil-mount scenario.

So far the result is not good enough as expected.

Here is the CFG I'm testing right now.

I copy the CFG from People Tracking demo for IWRL6432BOOST, modified the sensor position, boundaries, and tracking parameter (original one cause a lot of ghost object).

sensorStop 0
channelCfg 7 3 0
chirpComnCfg 16 0 0 128 4 28 3
chirpTimingCfg 6 32 0 40 60
frameCfg 2 0 200 64 100 0
antGeometryCfg 0 0 1 1 0 2 0 1 1 2 0 3 2.418 2.418
guiMonitor 2 3 0 0 0 1 0 0 1 0 0
sigProcChainCfg 16 8 3 2 8 8 1 0.3
cfarCfg 2 8 4 3 0 8.0 0 0.5 0 1 0 0
aoaFovCfg -60 60 -40 40
rangeSelCfg 0.1 4
clutterRemoval 1
compRangeBiasAndRxChanPhase 0.0 1.00000 0.00000 -1.00000 0.00000 1.00000 0.00000 -1.00000 0.00000 1.00000 0.00000 -1.00000 0.00000
adcDataSource 0 adc_data_0001_CtestAdc6Ant.bin
adcLogging 0
lowPowerCfg 0
factoryCalibCfg 1 0 40 0 0x1ff000
boundaryBox -3 3 -2 2.5 -0.5 3
sensorPosition 0 0 2.8 0 90
staticBoundaryBox -2.5 2.5 -1.5 2.3 0 2.5
gatingParam 3 2 2 2 4
stateParam 3 50 100 100 5 300
allocationParam 10 12 0.1 2 0.5 20
maxAcceleration 0.4 0.4 0.1
trackingCfg 1 2 100 6 61.4 191.8 100
presenceBoundaryBox -3 3 -2 2.5 -0.5 3
baudRate 1250000
sensorStart 0 0 0 0

When I'm searching the solution to fine tune the CFG, I notice that in the Overhead 3D People Tracking User Guide, it provides different CFGs for Wall-mount and Ceil-mount scenarios and describes that they need different way of estimating the angle of each detected dynamic point (3D_people_tracking_detection_layer_tuning_guide.pdf).

I am curious about if IWRL6432BOOST required same adjustment and if TI provides reference CFG for Ceil-mount for testing?