This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843AOPEVM: ADC Raw data capture using DCA1000 CLI commands on ubuntu system

Part Number: AWR1843AOPEVM
Other Parts Discussed in Thread: AWR1843AOP

Tool/software:

Hi TI,

We are working on AWR1843AOP EVM board with DCA1000 for raw data collection using DCA1000 CLI commands on ubuntu system. It is working fine with wine on intel based X86 architecture, with 8 GB RAM, ubuntu 22.04 OS. But the same thing is not working on ARM architecture, ubuntu 20.04, 8GB RAM with wine as well as without wine.

On ARM based system when we give START_Record command through CLI it opens the terminal and it automatically exits the terminal without giving a success message. Also after giving STOP command we get Timeout      error. We also tried increasing the time but it doesn't work. 

We are not able to figure out whether it is the compatibility issue or RAM issue or something else.


Please suggest the solution.

With Regards,

Rashmika Thota