This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMAG5170: Required wait time when triggering samples from CONFIG Mode

Part Number: TMAG5170

Tool/software:

When the TMAG5170 is in Config mode and a sample is triggered and the data is ready in the output registers (as indicated by STAT7 through STAT4 in the Figure 7-11 in the data sheet), how long should the host wait before triggering another sample? The TMAG returns to Config mode after the sample is taken, but it is unclear when the device is ready to be triggered again. This information would dictate what the maximum sample rate is when in config mode.